imx6 & imx8 mipi csi terminal resistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 & imx8 mipi csi terminal resistor

Jump to solution
1,790 Views
alex_li
Contributor II

I have some question about mipi csi terminal resistor .

In imx6 SDB schematic, there isn't any terminal resistor in MIPI CSI port,same as imx8qm VALIDATION CPU CARD. Does not need these terminal resistores or already integrated in SOC?

pastedImage_2.png

pastedImage_1.png

Thank!

0 Kudos
Reply
1 Solution
1,655 Views
igorpadykov
NXP Employee
NXP Employee

Hi min

yes terminal resistores are already integrated in SOC.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
1,656 Views
igorpadykov
NXP Employee
NXP Employee

Hi min

yes terminal resistores are already integrated in SOC.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,655 Views
95315858
Contributor I

hello,Igorpadykov, Could you tell me which document refer to MIPI internal information? Thanks

0 Kudos
Reply
1,655 Views
alex_li
Contributor II

Dear igor:

   These resistores need be enabled / disabled by SW or always active?

Thanks!

0 Kudos
Reply
1,655 Views
igorpadykov
NXP Employee
NXP Employee

they are always active

 

Best regards
igor

0 Kudos
Reply
1,655 Views
alex_li
Contributor II

Thanks very much!

0 Kudos
Reply