imx6 i2s audio playback issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 i2s audio playback issue

1,621 次查看
satishkumarchal
Contributor I

Hi All,

I have a customized board which has imx6 in it with android jellybean 4.2.2 version.

when i play a stream which has sine 10 tones in it (sampled at 44 KHz) through i2s and when i captured the same thing through mic ( or line in cable) with windows sound recorder.

In stream,time interval between each tone is 1sec. when i observe the recorded stream it has 10 tones in it But time interval between each tone is 0.984 sec.

If I take the dump before rendering, am getting same as the original stream ( time interval is 1sec ).

Is this i2s codec problem which is rendering more than what we have given ?

What could be the cause for the issue, Can any one help me ?

Thanks in advance.

Note :- Rendering Sampling frequency is 48 KHz.

Regards,

csk

Message was edited by: satish kumar challa

标记 (4)
0 项奖励
回复
1 回复

984 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi satish,

    0.984 sec is very close to 1 sec, It should not affect audio playback, I feel the phenomena should be generated by clock precision.

Regards,

Weidong

0 项奖励
回复