imx6 gstreamer hdmi image display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 gstreamer hdmi image display

2,663 Views
shencheng
Contributor I

hi all i used followed to display image in my application

gst-launch filesrc location="pngimage"  ! pngdec ! imagefreeze ! mfw_isink display=hdmi &

then kill the progress to prepare next image display 

everytime the image display with some distortion start then display correct image, my application needs to display different image thousands time so this distortion is not acceptable and it cant displayed on my monitor shows "single input is not 1920x1080 60hz resultion" 

i wonder to ask is there anyway to create a pipeline with gstreamer to display a static image keep it refresh like a video and i can change the image when i want?

sorry about my english

Labels (3)
0 Kudos
Reply
3 Replies

1,925 Views
igorpadykov
NXP Employee
NXP Employee

Hi shen

please try pipelines described in attached Linux Guide

sect.7 Multimedia with nxp linux releases on

i.MX 6 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,925 Views
shencheng
Contributor I

sorry, any detail of it?

i read the pdf and dont know what should i do

0 Kudos
Reply

1,925 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply