imx6 flexcan question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 flexcan question

1,319件の閲覧回数
angelo_d
Senior Contributor I

Hi all,

just testing some communications using PEAK usb CAN simulator.

I have seen that i can communicate up to 2Mbit/sec. Is this ok ?

With

ip link set can0 up type can bitrate 2000000

on both sides and using cangen tool.

Is it by the way this speed safe to be used ? At least, signals seems still good.

ラベル(2)
3 返答(返信)

1,211件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

according to sect.26.1.2 FLEXCAN Module Features

i.MX 6Dual/6Quad Applications Processor Reference Manual

"..bit rate up to 1 Mb/sec"

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,211件の閲覧回数
angelo_d
Senior Contributor I

Hi Igor.

But i am going at 2Mhz·

Measured single bitwidth is 500nsecs.

So looks like flexcan can spin over can2.0b.

1,211件の閲覧回数
angelo_d
Senior Contributor I

Would be nice if someone in the future may confirm my finding.

pastedImage_1.png

0 件の賞賛
返信