imx6 eMMC flash issue using mfg tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 eMMC flash issue using mfg tool

1,723 次查看
shivashankar
Contributor II

Hi Team,

We are using i.MX6D processor on a Nano SOM and I have a eMMC flash on it.

We are unable to flash it using mfg tool and it is getting stuck as shown in the attachment.

The mfg tool is working fine when I flash the SD card but fails for eMMC.

The boot configurations are set correctly. Kindly help me resolve the issue.

 

Regards,

Shiva Shankar K.

标记 (1)
0 项奖励
回复
1 回复

1,715 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shiva

 

this may be hardware issue, one can try to test emmc with baremetal test and check emmc signals with oscilloscope

https://github.com/RT-Thread/rt-thread/blob/master/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/usdhc/te...

 

Best regards
igor

0 项奖励
回复