imx6 duallite configuration file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 duallite configuration file

1,346 Views
shankovai
Contributor III

Hello support team,

Kindly refer the attached snapshot machine.png from the folder meta-freescale

configuration file for imx6dlsabresd is not available in the meta-freescale. why the conf file is not included?

  Can i use  imx6qdlsabresd.conf for imx6dl?

kindly give your suggestion

thank you

 

 

 

 

 

 

 

0 Kudos
Reply
1 Reply

1,334 Views
shankovai
Contributor III

n the meta-imx layer, i.MX provides new or updated machine configurations that overlay the meta-freescale machine
configurations. These files are copied into the meta-freescale/conf/machine directory by the imx-setup-release.sh script.

 

kindly refer the attachment meta-imx.png

then for the machine setup do i need to refer meta-imx/meta-bsp/conf/machine.

please confirm

0 Kudos
Reply