Hello
FlexCAN does not work on NAND binary. (But, goot work on SDCARD binary)
Please see the attached booting log.
'imx6dl-sabreauto-gpmi-weim.dts' file is bellow.
| /* * Copyright (C) 2014 Freescale Semiconductor, Inc. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include "imx6dl-sabreauto.dts" &ecspi1 { /* pin conflict with weim */ status = "disabled"; }; &flexcan1 { /* kyb_16 */ status = "okay"; }; &flexcan2 { /* max7310_c on i2c3 is gone */ status = "disabled"; }; &gpmi { status = "okay"; }; &i2c3 { /* pin conflict with weim */ status = "disabled"; }; &uart3 { /* pin conflict with gpmi and weim */ status = "disabled"; }; &usbh1 { /* max7310_b on i2c3 is gone */ status = "disabled"; }; &usbotg { dr_mode = "peripheral"; status = "disabled"; // _16 }; &weim { pinctrl-assert-gpios = <&gpio5 4 GPIO_ACTIVE_LOW>; status = "okay"; // _16 }; |
Original Attachment has been moved to: 1.booting-log.txt.zip
Original Attachment has been moved to: imx6qdl-sabreauto.dtsi.zip
Original Attachment has been moved to: imx6dl-sabreauto.dts.zip
Original Attachment has been moved to: imx6qdl.dtsi.zip
解決済! 解決策の投稿を見る。
Hi yunbaekim
from log seems flexcan driver is registered ok, no errors.
Could you elaborate how it does not work on NAND, any
errors messages, dmesg output ?
Also had you tried with latest L4.1.15 BSP :
Board Support Packages (35)
L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yunbaekim
from log seems flexcan driver is registered ok, no errors.
Could you elaborate how it does not work on NAND, any
errors messages, dmesg output ?
Also had you tried with latest L4.1.15 BSP :
Board Support Packages (35)
L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------