[imx6 dl] FlexCan does not work on NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[imx6 dl] FlexCan does not work on NAND

ソリューションへジャンプ
1,282件の閲覧回数
yunbaekim
Contributor II

Hello

FlexCAN does not work on NAND binary. (But, goot work on SDCARD binary)

Please see the attached booting log.

 

'imx6dl-sabreauto-gpmi-weim.dts' file is bellow.

/*
  * Copyright (C) 2014 Freescale Semiconductor, Inc.
  *
  * This program is free software; you can redistribute it and/or modify
  * it under the terms of the GNU General Public License version 2 as
  * published by the Free Software Foundation.
  */

#include "imx6dl-sabreauto.dts"

&ecspi1 {
  /* pin conflict with weim */
  status = "disabled";
};
&flexcan1 {
  /* kyb_16 */
  status = "okay";
};
&flexcan2 {
  /* max7310_c on i2c3 is gone */
  status = "disabled";
};

&gpmi {
  status = "okay";
};

&i2c3 {
  /* pin conflict with weim */
  status = "disabled";
};

&uart3 {
  /* pin conflict with gpmi and weim */
  status = "disabled";
};

&usbh1 {
  /* max7310_b on i2c3 is gone */
  status = "disabled";
};

&usbotg {
  dr_mode = "peripheral";
  status = "disabled"; // _16
};

&weim {
  pinctrl-assert-gpios = <&gpio5 4 GPIO_ACTIVE_LOW>;
  status = "okay"; // _16
};

Original Attachment has been moved to: 1.booting-log.txt.zip

Original Attachment has been moved to: imx6qdl-sabreauto.dtsi.zip

Original Attachment has been moved to: imx6dl-sabreauto.dts.zip

Original Attachment has been moved to: imx6qdl.dtsi.zip

ラベル(1)
1 解決策
1,106件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yunbaekim

from log seems flexcan driver is registered ok, no errors.

Could you elaborate how it does not work on NAND, any

errors messages, dmesg output ?

Also had you tried with latest L4.1.15 BSP :

Board Support Packages (35)

L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,107件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yunbaekim

from log seems flexcan driver is registered ok, no errors.

Could you elaborate how it does not work on NAND, any

errors messages, dmesg output ?

Also had you tried with latest L4.1.15 BSP :

Board Support Packages (35)

L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------