Please help me to save the main board.
The main boards I use are imx6q, kernel 3.0.35, Android 4.4.2
I use the fuse mechanism to prepare for the production of the factory.
echo 0x00005860 >/sys/fsl_otp/HW_OCOTP_CFG4
echo 0x00000010 >/sys/fsl_otp/HW_OCOTP_CFG5
Then it is true that the device can be used.
But I accidentally operated on the following statement:
echo 0x0000787B >/sys/fsl_otp/HW_OCOTP_CFG4
Then it operates again.
echo 0x00005860 >/sys/fsl_otp/HW_OCOTP_CFG4
cat /sys/fsl_otp/HW_OCOTP_CFG4
The result is 0x0000787B, not 0x00005860.
Then the system can't start.
I used mfgtool to burn a uboot that was started from memory, modified the command imxotp, forced to write to 0x00005860, and used the command operation as follows:
MX6Q SABRESD U-Boot >imxotp blow --force 5 0x5860
Current fuse at (index: 0x5) value: 0x787B
Blowing fuse at index: 0x5, value: 0x5860
Reloading shadow registers...
Operation succeeded fuse at (index: 0x5) value: 0x787B
But it still doesn't become 0x00005860.
MX6Q SABRESD U-Boot >imxotp read 0x5
Reading fuse at index: 0x5
Fuse at (index: 0x5) value: 0x787B
Or enter the system, as follows:
echo 0x00005860 >/sys/fsl_otp/HW_OCOTP_CFG4
The result is 0x0000787B, not 0x00005860.
I can't help me. Please help me.
How to remove its value or write to 0x5860.
What's the matter with this situation?
Online wait!
Help, thank you!