imx6 android6.0 hotspot open error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 android6.0 hotspot open error

883 次查看
sunyd
Contributor I

11-14 11:37:15.888 557 601 D wifi : set interface wlan0 flags (UP)
11-14 11:37:15.888 557 601 D wifi : Did set static halHandle = 0x0
11-14 11:37:15.888 557 601 D wifi : halHandle = 0x0, mVM = 0xb4d3c000, mCls = 0x200b12
11-14 11:37:15.888 557 601 E WifiNative-HAL: Could not start hal
11-14 11:37:15.888 557 601 E WifiStateMachine: Failed to start HAL

11-14 11:37:15.938 204 556 D SoftapController: SoftAP started successfully
11-14 11:37:15.938 1298 1298 E SoftapController: no specific driver vendor
11-14 11:37:15.938 1298 1298 E SoftapController: execl failed (Cannot assign requested address)
11-14 11:37:15.938 1298 1298 E SoftapController: SoftAP failed to start
11-14 11:37:15.939 557 1297 E WifiStateMachine: Exception in softap start java.lang.IllegalStateException: command '79 softap startap' failed with '402 79 SoftAP command has failed'
11-14 11:37:15.942 1298 1298 E SoftapController: SoftAP is not running
11-14 11:37:15.945 1298 1298 D SoftapController: Softap fwReload - Ok
11-14 11:37:15.989 1298 1298 D SoftapController: SoftAP started successfully
11-14 11:37:15.989 1299 1299 E SoftapController: no specific driver vendor
11-14 11:37:15.989 1299 1299 E SoftapController: execl failed (Cannot assign requested address)
11-14 11:37:15.989 1299 1299 E SoftapController: SoftAP failed to start
11-14 11:37:15.990 557 1297 E WifiStateMachine: Exception in softap re-start java.lang.IllegalStateException: command '83 softap startap' failed with '402 83 SoftAP command has failed'
11-14 11:37:15.991 557 557 E WifiController: WifiControllerSoftAP start failed

description:wifi work well,but hotspot can't be open? please help me resolve this error

thank you;

标签 (1)
0 项奖励
回复
1 回复

790 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sunid

such wifi guidelines should be provided by vendors of used wifi modules.

For murata devices supported in nxp software one can look at documentation provided on

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复