imx6 android 4.3 build and gstreamer 1.2.x not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 android 4.3 build and gstreamer 1.2.x not working

1,774 次查看
alokkumar
Contributor III

Hi,

I wanted to test imx6  freescale android box (utilite and nitrogen6x) which has android 4.3 with gstreamer tutorial 3. Though it was working with decodebin pipeline (androidmedia)  and android 4.2.

It was getting following error.

05-10 23:27:05.670 E/BufferQueue( 2462): [SurfaceView] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

05-10 23:27:05.700 W/GStreamer+bufferpool( 3289): 0:04:10.883391696 0x416518c0 gstbufferpool.c:632:gst_

buffer_pool_set_config:<eglimagebufferpool1> can't change config, we are active
05-10 23:27:05.700 W/GStreamer+bufferpool( 3289): 0:04:10.883543029 0x416518c0 gstbufferpool.c:632:gst_buffer_pool_set_config:<eglimagebufferpool1> can't change config, we are active
05-10 23:27:05.700 E/GStreamer+amcvideodec( 3289): 0:04:10.884113029 0x416518c0 gstamcvideodec.c:806:gst_amc_video_dec_fill_buffer:<amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2> Slice height not set
05-10 23:27:05.700 W/GStreamer+amcvideodec( 3289): 0:04:10.884820362 0x416518c0 gstamcvideodec.c:1314:gst_amc_video_dec_loop:<amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2> error: Invalid sized input buffer
05-10 23:27:05.700 I/tutorial( 3289): Error received from element amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2: Could not configure supporting library.
05-10 23:27:05.700 E/GStreamer+amcvideodec( 3289): 0:04:10.886152696 0x657528c0 gstamcvideodec.c:1683:gst_amc_video_dec_handle_frame:<amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2> Downstream returned not-negotiated
05-10 23:27:05.700 W/GStreamer+qtdemux( 3289): 0:04:10.886591362 0x65752860 qtdemux.c:4404:gst_qtdemux_loop:<qtdemux0> error: streaming stopped, reason not-negotiated

Any suggestions are highly appreciated.

Thanks

Alok

标签 (2)
0 项奖励
回复
2 回复数

1,221 次查看
YixingKong
Senior Contributor IV

Alok

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复

1,221 次查看
YixingKong
Senior Contributor IV

Alok

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复