I have a Qt5-application using eglfs that uses fb0. I want to alpha-blend it with an overlay buffer filled with a color. What is the proper/best way to solve this?
I tried creating an ipu_task with /dev/fb0 as input, an overlay buffer, and /dev/fb1 as output. It does not work, however, and I'm unsure if I'm on the right track.
If I should use /dev/fb1 at all, what is the proper way of setting the same modes on /dev/fb0 and /dev/fb1? Based on the output from fbset on /dev/fb0 I ran "fbset -fb /dev/fb1 -g 800 480 800 1440 32", which seemed to work, but is that the proper way to do it? Is that what I should do if/when I want to switch to another display timing?
Turned out I was overcomplicating this. I did not need an ipu_task at all. After filling /dev/fb1 with the desired color and unblanking it, I just did this.
struct mxcfb_gbl_alpha a;
a.enable = 1;
a.alpha = alpha_value;
int err = ioctl(fd_fb, MXCFB_SET_GBL_ALPHA, &a);
if (err) {
printf("Could not set alpha\n");
return -1;
}
Hi Anders
may be helpful to look at usage blending examples in attached
Linux Guide sect.7.3.16 Video composition, sect.8.2 G2D-imx-samples and
ipu-examples release notes - v0.1
[meta-freescale] IPU alpha blending problems on mx6
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------