Hi,
I am in a process of migrating our imx6qpsabreauto morty build system to rocko and I am facing issue with generating u-boot image for eimnor.
I found like now the machine file got changed from imx6qpsabreauto to imx6qdlsabreauto
But I am not bale to generate eimnor image there is no option to specify UBOOT_CONFIG
ERROR: Nothing PROVIDES 'u-boot-fslc'
u-boot-fslc was skipped: You cannot use UBOOT_MACHINE and UBOOT_CONFIG at the same time.
Is it possible to specify u-boot to be build is for EIM-NOR without doing any extra patch in config files ?
Is u-boot-imx available for yocto rocko ?
latest nxp official linux bsp Linux 4.9.11_1.0.0 described in
https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS
Best regards
igor
Hi Igor,
As per the release note L4.9.11_1.0.0-ga 06/2017 Its says Yocto Morty version as the latest.
Does Yocto Rocko version bsp is released ?
what is the latest official Freescale support Yocto version ?
I am still facing the same error when i try to build u-boot with yocto rocko.
#bitbake u-boot-imx-mfgtool
ERROR: Nothing PROVIDES 'u-boot-imx-mfgtool'
u-boot-imx-mfgtool was skipped: You cannot use UBOOT_MACHINE and UBOOT_CONFIG at the same time.
Regards
Sijil CV
Hi Sijil
please look at
difference between Yocto Community BSP and Freescale BSP Release
nxp official bsps are described on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi sijil
for "u-boot-fslc" (community version of uboot) issues please post on
uboot mail list U-Boot Info Page
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------