We are operating iMX6 USB OTG port in device mode. We are able to connect the host device and start the transfer.
But after few seconds of working, imx6 USB OTG port is not responding to IN packet sent by Host device.
Based on our understanding, USB device controller should send atleast the NAK packet for the IN token from the Host?
Are there any known issues in imx6? Could you please advise on how to debug this issue further?
Are there any test daemons available to check the USB transfer between PC and imx6 USB device?
Hi Karthigeyan
I would recommend to check boar with SDK USB test
i.MX 6Series Platform SDK
: Bare-metal SDK
also issue may be related to DDR errors, one can update calibration
settings
https://community.freescale.com/message/331721#331721
https://community.freescale.com/docs/DOC-96412
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your comments. Please note that this issue is not happening in the standalone setup.
We could re-produce this issue only when the Graphics/GUI engine is running in parallel.
Problem:
Imx6 USB OTG port is configured in device mode. We are able to connect the USB Host device and do the data transfer.
But after few packets data transfer, imx6 USB device controller is not responding to PING and IN token sent by Host device.
Refer the attached snapshot for the details. As per our understanding , responding to IN token is done the USB core in the HW and not in the SW.
What we need from freescale:
Hi Karthigeyan
definitely this is DDR issues or power supplies (ripples, spikes).
Check them all carefully.
Graphics/GUI engine produces tremendous current spikes.
Just for test you can decrease operating frequency.
Best regards
chip
Thanks for the feedback. Could you please advise on which operating frequency to reduce and check and how much? Is it core clock or GPU clock or DDR clock?
Please advise
Hi Karthigeyan
try to change them all: core, DDR frequencies
and check by oscilloscope power lines.
200,400MHz may as test points.
Best regards
chip
Thanks for the feedback. Are you referring to check USB VBus power line or Power lines to imx6 ?
We have reduced the CPU clock to 400mhz , but still the same issue occurs.
Need few clarifications:
1.You have mentioned the problem is due to DDR /Power supplies. Could you please help us on how you are correlating the above mentioned USB controller behavior with DDR/Power supplies?
2.As mentioned in the above logs , the imx6 USB OTG controller is not reponding to IN and PING packets. As per our understanding, this is supposed to be done by the HW USB core itself and not by the USB SW driver ? Is it correct?
I meant power lines to imx6.
1. correlation from practice. usually this is caused by
DDR errors or power supply ripples.
2. this may be caused both.
Also it may be suugested to run minimal linux image and check
behaviour.
Thanks for the feedback
>>On your suggestion" Also it may be suugested to run minimal linux image and check behaviour"
We have the following TWO observations
1. This issue is not happening if we reduce the GUI engine processing in our carplay application
Apple iPhone (acting as USB Host)-<>imx6 (acting as device).
2. For debugging purpose, we have tested the data transfer between PC and imx6. In this setup, USB data transfer is working even if we DONT reduce the GUI engine processing
PC (acting as USB Host)-<>imx6 (acting as device).
Please advise.
Still I think that this may happen due to some
power/noise issues.
Also this may be caused by Apple iPhone - probably its
USB protocol is not correctly handled by i.MX6.
I think you can check with Apple iPhone vendor what can be
problem.
We have done requested tests
-There is no problem with Power
-There is no problem with DDR
-There is no problem with Apple device since the functionality works when we reduce the graphics processing which uses GPU/IPU drivers.
During the normal condition, Are there a possibility that imx6 not responding to IN & PING packet when the imx6 device operating in device mode?
This issue is pending for long time. Could you please support us for the next steps?
To be able to support that, we should be able
to reproduce this issue. Could you provide steps to reproduce
it using Freescale reference board/BSP and some commonly
used USB device.
It may not be easy to port our SW to freescale reference board. It is huge effort for us. Kindly provide the alternate options.
Please answer my question in previous context :" During the normal condition, Are there a possibility that imx6 not responding to IN & PING packet when the imx6 device operating in device mode?"
In other way, if imx6 should not MISS to respond to even ONE IN & PING packet. If it is missing, then it is considered as abnormal. Is this statement true?
Acknowledging IN& PING packet can be done automatically by mx6 USB core without software intervention. Is our understanding correct?. If not , please provide the details
Hi Karthigeyan
unfortunately some problems can be found only running real
board at hand. BTW there is another support path: you can apply to Freescale Professional Services:
http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL
>:" During the normal condition, Are there a possibility that imx6 not responding to IN & PING
>packet when the imx6 device operating in device mode?"
There is no such possibility, provided that hardware is OK and running correctly written software.
>In other way, if imx6 should not MISS to respond to even ONE IN & PING packet. If it is
>missing, then it is considered as abnormal. Is this statement true?
Yes.
>Acknowledging IN& PING packet can be done automatically by mx6 USB core without
>software intervention. Is our understanding correct?. If not , please provide the details
Corect. Provided that hardware is OK and running correctly written software.
Best regards
chip
Could you please clarify the meaning "running correctly software" written in the above email?
We are using USB drivers provided by freescale. Are there any known issue related to this?
Hi Karthigeyan
as far as remember you answered before:
"It may not be easy to port our SW to freescale reference board."
So seems you changed software and it is not possible to answer
what is wrong in it. So I asked you provide steps to reproduce
issue using Freescale reference board/BSP and some commonly
used USB device.
Best regards
chip
We have not changed any SW in the USB driver which is provided by freescale. What i meant is porting to our graphics engine is difficult
Please let us know your views considering this.
I think you can build minimal image
(without "our graphics engine") with
Freescale BSP and test this case on
Freescale reference board.