imx6 UART issue on 5.4.24 kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 UART issue on 5.4.24 kernel

跳至解决方案
3,075 次查看
zc_tee
Contributor III

Hi all,

I am porting my I.MX6 platform kernel from 4.9.11 to 5.4.24, and face some weird issue on the UART port

after i port the code and my device tree, I manage to boot up my machine. Then I tried to read some data from another subcpu which is connected to ttymxc2. 

In console, I tried to cat /dev/ttymxc2, but it returns me with some text that seems like system related information as below:

zc_tee_0-1603083379260.png

I tried to do a stty then cat, it returns me with another type of information, which seems to be like cat /proc/filesystems plus something else as below:

zc_tee_1-1603083564920.png

I cannot understand why is this happening. It seems like the ttymxc device is mixed up with /proc/ information. Can anybody advise? 

One thing is that the system is working fine in kernel 4.9.11. Only change is changing the kernel from 4.9.11 to 5.4.24.

By the way, i am using same bootloader 2017.03 for both the 4.9.11 and 5.4.24 kernel. I suppose 5.4.24 kernel can work well with 2017.03 uboot?

Thank you.

Regards,

Tee

 

 

0 项奖励
回复
1 解答
3,052 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tee

 

usually dma is disabled for console port.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,065 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tee

 

you are right, reason may be in uboot, recommended to use

uboot version (v2020.04) as listed in Release Notes of each BSP described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=imx_v2020.04_5.4.24_2.1.0

 

Best regards
igor

0 项奖励
回复
3,062 次查看
zc_tee
Contributor III

Hi Igor,

After doing some searching online, i tried to disable the serial port dma in device tree

zc_tee_0-1603092574958.png

Then my machine's UART port works.

I think i will disable the UART dma for now and test further. Do you forsee any issue disabling the UART's dma?

Regards,

Tee

 

 

0 项奖励
回复
3,053 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tee

 

usually dma is disabled for console port.

 

Best regards
igor

0 项奖励
回复
3,042 次查看
zc_tee
Contributor III

Hi Igor

Thank you. I will proceed with disabling UART dma.

0 项奖励
回复