imx6 Trustzone: How to boot smp kernel in normal world?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 Trustzone: How to boot smp kernel in normal world?

3,638件の閲覧回数
shenchun
Contributor I

I try implement trustzone on collage-mx6q board, now there is a simple secure kernel and secure os can work.

after secure parts startup, it will switch to non-secure status to run uboot and kernel.

now the uboot can work, but the kernel can work only without SMP setting , it means I can only use one processor.

part log:

Linux version 3.0.35-2026-geaaf30e-g679aa00-dirty

......

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: failed to come online

CPU1: failed to come online

I setting some parts what need to do in my opinion.

1. CSU    all reg setting 0x00ff00ff

2. SCU    SCU Access Control Register is 0xf, SCU Non-secure Access Control Register is 0xfff

3. GIC-v1     ICDISR0-n reg, PPI and SGI all setting non-secure,, SPI almost setting non-secure(except some need secure)

4. some reg in cp15 and PL310 can not setting in non-secure, i have use smc to fix it.

but i have no idea about "CPU1: failed to come online"

is there any suggestion  about smp kernel can not work?

ラベル(5)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,687件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to Chapter 3 (Multicore Startup) of “iMX6_Firmware_Guide.pdf” in the Platform SDK
regarding details of multicore using. 

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&fpsp=1&WT_TYPE=Sn...

In particular, please check SRC accessibility for normal world. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,687件の閲覧回数
shenchun
Contributor I

Hi:Yuri

The SRC accessibility for normal world is ok,I try it long time ago,

because the datasheet has nothing about it's access permission secure or non-secure

so i think it doesn't matter about my question.

thank you for your response

let's keep on discussing it

Best Regards

steven-shen

0 件の賞賛
返信