Hi,
I have imx6q sabresd board.
With the help of the community, I was able to set up the SPI driver.
However, the spi data does not look right.
on the imx6q sabresd board
Is the spi driver not properly configured?
If the settings are wrong, how can I fix them?
Also, is there any C code to read this spi data and save it in file form?
My final goal is to save the spi data I am reading on the imx6sabresd board to a file.
Please help me.
Best regards,
kangta
Hi kangta
please check
java - Read received data via /dev/spi* - Stack Overflow
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------