[imx6] RS485 could be supported on Imx6 series ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx6] RS485 could be supported on Imx6 series ?

Jump to solution
7,073 Views
keres_kim
Contributor II

Hi imx-developers,

Good day !

It's simple. Could imx6 chipset support RS485 ?

There are many related questions posted on this community about RS485.

Many patch codes exist as well but I not sure which one would be trusted.

Would you somebody tell us which patch code works well on rs485 ?

thank you. 

0 Kudos
Reply
1 Solution
3,952 Views
igorpadykov
NXP Employee
NXP Employee

Hi keres

RS485 is currently not supported by the imx serial driver, however

some folks seems added RS485 support to the imx serial driver.

http://marc.info/?l=linux-kernel&m=142366865609389&q=raw

http://www.spinics.net/lists/linux-serial/msg15795.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
3,952 Views
raje_embd13
Contributor I

I had similar requirement right now. Can help on this.  Is any patch which support RS485 on Imx6 processor ?

0 Kudos
Reply
3,952 Views
marcocavallini
Contributor V
0 Kudos
Reply
3,953 Views
igorpadykov
NXP Employee
NXP Employee

Hi keres

RS485 is currently not supported by the imx serial driver, however

some folks seems added RS485 support to the imx serial driver.

http://marc.info/?l=linux-kernel&m=142366865609389&q=raw

http://www.spinics.net/lists/linux-serial/msg15795.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,952 Views
keres_kim
Contributor II

Dear Igor,

Thank you for your response.

Patch code from "Marc" is working well.

http://marc.info/?l=linux-kernel&m=142366865609389&q=raw

RS485 TX data has verified successfully,But not RX. I'm still checking on it.

Have a nice day ~~

0 Kudos
Reply
3,952 Views
LPs
Contributor III

Hi Kim,

   did you managed to make the RX working?

0 Kudos
Reply