Hi,
We are planning to use imx6Quad core processor for application;
Could any one suggest which is the right Evaluation board to procure to start with.
Is the MCIMX6Q-SDP is the right one to start ?
Our requirements are listed down,
Core : Quad
PCIe interface – Required 2 (can provide a PCI bridge if required)
Interfaces required:
CAN BUS
USB
UART - 3 Nos.
SDIO -> SDIO card Interface / eMMC Interface
Gigabit Ethernet -> 10/100/1000 GBE
GPIO -> Pins with Interrupt Capability/ General IO
Display -> TFT/ Touch Controller
Thanks & Regards
Lijo Thomas
Hi Lijo
Sabre Auto best fit, since MCIMX6Q-SDP has not CAN
SABRE|Automotive-Infotainment|i.MX6|Freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks igor for the reply,
Do you have any other EB board to suggest, which has all the peripherals I mentioned
Regards
Lijo Thomas
Hi Lijo
there are no other FSL reference boards with such
characteristics.
Best regards
igor