imx6 MIPI input 60fps

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 MIPI input 60fps

跳至解决方案
1,793 次查看
zhencongtee
Contributor III

Hi,

May I know does the i.mx6 Solo support camera MIPI input up to 60fps at 1024x768 resolution?

Thank you.

Regards,

Zhen Cong Tee

标记 (3)
0 项奖励
回复
1 解答
1,370 次查看
Yuri
NXP Employee
NXP Employee

MIPI CSI-2 supports from 80 Mbps to 800 Mbps speed per data lane.

The CSI-2 Receiver core can manage one clock lane and up to two data lanes.

Each i.MX 6Solo/6DualLite processor has two lanes.

 
Basically it is enough to support 60fps at 1024x768.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,371 次查看
Yuri
NXP Employee
NXP Employee

MIPI CSI-2 supports from 80 Mbps to 800 Mbps speed per data lane.

The CSI-2 Receiver core can manage one clock lane and up to two data lanes.

Each i.MX 6Solo/6DualLite processor has two lanes.

 
Basically it is enough to support 60fps at 1024x768.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复