imx6 L4.9.11 can work with gstreamer-0.10?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 L4.9.11 can work with gstreamer-0.10?

ソリューションへジャンプ
970件の閲覧回数
westbrook
Contributor III

Hello guys,

Can I use imx6 L4.9.11 BSP with gstreamer-0.10? I checked this yocto L4.9.11, it use gstreamer-1.0, If I downgrade to gstreamer-0.10, will it work?

Thank you

Best Regards,

Xiao

ラベル(3)
0 件の賞賛
返信
1 解決策
842件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xiao

supported gstreamer version is 1.10.4 as described in attached Release

Notes, as for gstreamer-0.10, it was not tested and its operation is not guaranteed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
843件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xiao

supported gstreamer version is 1.10.4 as described in attached Release

Notes, as for gstreamer-0.10, it was not tested and its operation is not guaranteed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
842件の閲覧回数
westbrook
Contributor III

Hi igor,

Thanks for your answer.

Our application use old gstreamer-0.10, so if we use this L4.9.11, the application need to update to gstreamer-1.10? Anything we can refer to the difference between gstreamer-0.10 and 1.10?

Thank you.

Best Regards,

Xiao

0 件の賞賛
返信
842件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xiao

yes with L4.9.11 the application needs to update to gstreamer-1.10, for

gstreamer usage one can look at Linux Guide included in documentation packages on link

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
842件の閲覧回数
westbrook
Contributor III

Hi Igor,

Thank you so much.

Best Regards,

Xiao

0 件の賞賛
返信