imx6 Horizontal inversion

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 Horizontal inversion

1,796 次查看
allen_kim1
Contributor I

Dear Community

i have a question about Horizontal inversion(horizontal flip) 

pastedImage_1.png

i know imx6's ipu has below IP block

Image converter , Image rotator 

IC and IRT has a  horizontal inversion 

my first question is how can i use that function of IC or IRT ?

what is best choice of IC or IRT ? 

pastedImage_2.png

i already 120 bit set to 1 , but movie clip is not changed 

i did some test with mxc_vpu_test.out program 

mxc_vpu_test.out has a option "-m" about mirror 

i have confirmed horizontal flip video with "-m 2" option 

but i  have a question VPU has a function about horizontal flip ? 

What is different IPU flip and VPU MIRROR ? it is my second question

Thansk BR

0 项奖励
回复
1 回复

1,448 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Allen

vpu and ipu are different blocks, vpu is processing

only video. For vpu mirror capability one can look at attached

VPU Linux Programming Manual sect.sect.3.2.1.12 MirrorDirection.

As for ipu one can look at examples on

ipu-examples release notes - v0.1 | NXP Community 

i.MX6 IPU and rotating a frame buffer | NXP Community 

seems it is possible to reuse rotate example for conversion it to mirror

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复