The GPU 2D/3D acceleration is not working in the Yocto qte-in-use-image. Looks like the "virtual/libgles2" and "-opengl es2 -openvg" are missing from imx6 in files qt4-embedded_4.8.4.bbappend and qt4-x11-free_4.8.4.bbappend, as shown below.
DEPENDS_append_mx5 = " virtual/kernel virtual/libgles2"
PACKAGE_ARCH_mx5 = "${MACHINE_ARCH}"
QT_GLFLAGS_mx5 = "-opengl es2 -openvg"
QT_CONFIG_FLAGS_append_mx5 = " -I${STAGING_KERNEL_DIR}/include/"
DEPENDS_append_mx6 = " virtual/kernel"
PACKAGE_ARCH_mx6 = "${MACHINE_ARCH}"
QT_CONFIG_FLAGS_append_mx6 = " -I${STAGING_KERNEL_DIR}/include/"
Adding "virtual/libgles2" and "-opengl es2 -openvg" for the imx6 as below resulted in the attached build errors.
DEPENDS_append_mx6 = " virtual/kernel virtual/libgles2"
PACKAGE_ARCH_mx6 = "${MACHINE_ARCH}"
QT_GLFLAGS_mx6 = "-opengl es2 -openvg"
QT_CONFIG_FLAGS_append_mx6 = " -I${STAGING_KERNEL_DIR}/include/"
What is the correct way to enable GPU 2D/3D acceleration for imx6 in the Yocto qte-in-use-image?
Original Attachment has been moved to: log.do_configure.951.zip
Accordingly to LeonardoSandovalGonzalez until now in the Dylan branch, the Yocto release does not have hardware support configured for Qt correctly.
But in the master-next testing branch, there is a patch that enables the use of the GPU and it works.
Note that this is a workaround, and soon will be outdated because these changes could soon be approved to the master branch, and later to the official release.
Take into account that this is a development branch which could have other bugs hidden, also it is recommended to join the mailing list as mentioned before for future questions.
In order to use this patch :
First start the repo from 'master' not dylan, then
create a new branch on sources/meta-fsl-arm from yocto/master-next, after this, setup the bitbake system and bake the image (qt-in-use-image). In Yocto words:
$: mkdir ~/bin$: curl https://dl-ssl.google.com/dl/googlesource/git-repo/repo > ~/bin/repo$: chmod a+x ~/bin/repoDownload the BSP source:$: PATH=${PATH}:~/bin$: mkdir fsl-community-bsp$: cd fsl-community-bsp$: repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b master$: repo sync
$: cd sources/meta-fsl-arm
$: git checkout -b master-next yocto/master-next
Once this has complete, you will have all you need. To start a build, do:$: . ./setup-environment build$: bitbake qt-in-use-image
Hi Francisco,
I followed your procedure as ,
$: mkdir ~/bin
$: curl https://dl-ssl.google.com/dl/googlesource/git-repo/repo > ~/bin/repo
$: chmod a x ~/bin/repo
$: PATH=${PATH}:~/bin $: mkdir fsl-community-bsp
$: cd fsl-community-bsp
$: repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b master
$: repo sync
$: cd sources/meta-fsl-arm
$: git checkout -b master-next yocto/master-next
$: MACHINE=imx51evk source setup-environment build
$: bitbake qte-in-use-image
but getting EGL initialization error. openGL is not working.is there is patch i need to apply for imx51?
Ravi,
Please post your question into the meta-freescale mailing list.
Thanks for the answer! The Freescale GPU still seems to not work with the image "qte-in-use-image" in master-next testing branch. When executing "/usr/bin/qtopia/demos/affine/affine -qws &" and then running "top" it shows "affine" is taking about 50% of the CPU. What is the advantages of "qt-in-use-image" vs. "qte-in-use-image"? I thought the "qte-in-use-image" was for embedded devices, thus the extra "e". And "qt-in-use-image" is slow because of x-windows overhead.
Yes, sorry it was a typo,
use qte-in-use-image
I followed your guidelines but qte-in-use-image still doesn't use opengl. Applications using opengl gives segmentation fault. I've got same effect on master and dylan branch. Could you post here any solution for this problem.
You are right. Please try the qte-in-use-image image instead. As you mentioned, the main difference between is the X11 system present on the qt-in-use-image. Take a look at the images recipes for more detail (fsl-community-bsp/sources/meta-fsl-demos/recipes-qt/images)
leo
I would encourage you to post this question to the Yocto Freescale mailing list, as Qt is not officially supported by Freescale. Francisco and our team here will certainly try to help but do keep in mind this is not a supported feature.
General information about the mailing list is at https://lists.yoctoproject.org/listinfo/meta-freescale
To post to this list, send your email to: meta-freescale@yoctoproject.org
thanks,
Ragan
I am working in order to solve this question.