imx6 FEC1 mii Marvell switch 88E6122 interface work in u-boot but not work in linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 FEC1 mii Marvell switch 88E6122 interface work in u-boot but not work in linux

1,412 Views
ValeriyUrmanov
Contributor I

1. have a custom board with imx6 chip and marvell 88e6122 switch (fec1-mii connection)

2. U-boot initialize pins, switch, FEC is up and i can ping remote host connected to switch.

3. Linux (openwrt kernel 5.4.85) starts and initialize fec as fixed-link. Linux  knows nothing about switch.  eth0 is up. I run tcpdump and can see ARP requests coming from the remote host.  I can see ARP responses on eth0 , but they are not come to remote machine. Also CPU  cant ping remote machine. So looks like in linux MII interface work only in one direction. 

where is a way to solve problem?

0 Kudos
4 Replies

1,130 Views
NARAYANASWAMY
Contributor I

Hi @ValeriyUrmanov ,

We are facing issue with marvell switch(6141) integration with i.MX7D

Please share your DTS file and kernel config.

Thank you in advance.

 

0 Kudos

1,380 Views
uvmbox
Contributor III

i build and image from yocto source  repo init -u https://source.codeaurora.org/external/imx/imx-manifest
-b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml . kernel 5.4.74. And it did not help. Switch did not recognize packets.

0 Kudos

1,397 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear ValeriyUrmanov,

 

The kernel version you are using is 5.4.85. We have not issued this version of BSP, so we have no reference BSP version for your problem.

However, we can recommend a direction for your reference

In our BSP, l5.4.70 is the closest to 5.4.85_ 2.30, you can download the source code of the kernel. Using fec_main.c (MAC driver) to replace the MAC driver in your kernel.

# git clone https://source.codeaurora.org/external/imx/linux-imx -b imx_5.4.70_2.3.0

Try it, please!

Have a nice day!

B.R,

weidong

0 Kudos

1,376 Views
uvmbox
Contributor III

IMG_20210617_102324.jpgIMG_20210617_102330.jpgIMG_20210617_102332.jpgIMG_20210617_103335.jpg

I checked MII interface TX and RX lines and found out the the the length of ARP request packet fec send to switch  in Linux  ( first picture ) two times shorter than the same paket fec send to switch in U-boot and length come from switch. So it looks like timing issue. What can be cause of it?

0 Kudos