imx6 DDR stress test getting stuck

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 DDR stress test getting stuck

418 Views
shivashankar
Contributor II

Hi,

We are using i.MX6D processor on a Nano SOM and a DDR mounted on it.
The DDR is NT6TL64T64CR from Nanya Technologies. 

We have generated the new u-boot after generating the new .inc file and it is booting fine.

But the DDR stress test getting stuck as attached.

 

Regards,

Shiva Shankar K.

Tags (1)
0 Kudos
1 Reply

409 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shiva

 

such issue may be related to hardware, may be recommended to check memory

connections and layout. Also if this happens on only one board, this may be caused by poor soldering.

 

Best regards
igor

0 Kudos