imx6 - Cannot establish a secure HDCP link in DVI mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 - Cannot establish a secure HDCP link in DVI mode

1,278件の閲覧回数
jonchaps
Contributor II

Hello,

We've encountered an issue where the imx6 is unable to successfully establish a secure HDCP link when the HDMI transmitter is operating in DVI mode. What appears to happen is that the HDCP negotiation process is performed and then shortly thereafter the secure connection is lost. This will repeat over and over every couple of seconds (corresponding closely with the typical HDCP link verification interval). When the HDMI link is operating in HDMI mode, everything works properly.

Any help would be greatly appreciated.

Thanks,

Jon

ラベル(2)
0 件の賞賛
返信
1 返信

967件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Perhaps, the issue concerns using HDMI-DVI converter :  HDMI interface

should not be used with a HDMI-to-DVI converter. It is needed to apply "true"

HDMI.

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信