imx6 - Cannot establish a secure HDCP link in DVI mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 - Cannot establish a secure HDCP link in DVI mode

1,254 Views
jonchaps
Contributor II

Hello,

We've encountered an issue where the imx6 is unable to successfully establish a secure HDCP link when the HDMI transmitter is operating in DVI mode. What appears to happen is that the HDCP negotiation process is performed and then shortly thereafter the secure connection is lost. This will repeat over and over every couple of seconds (corresponding closely with the typical HDCP link verification interval). When the HDMI link is operating in HDMI mode, everything works properly.

Any help would be greatly appreciated.

Thanks,

Jon

Labels (2)
0 Kudos
Reply
1 Reply

943 Views
Yuri
NXP Employee
NXP Employee

  Perhaps, the issue concerns using HDMI-DVI converter :  HDMI interface

should not be used with a HDMI-to-DVI converter. It is needed to apply "true"

HDMI.

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply