imx6 CAN wakes up Linux immediately

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 CAN wakes up Linux immediately

ソリューションへジャンプ
3,602件の閲覧回数
akbar123
Contributor III

Hi,

I can wake Linux up using UART by enabling its wakeup capability:

    $ echo enabled > /sys/class/tty/ttymxc0/power/wakeup

I have put Linux into sleep using the following command:

    $ echo mem > /sys/power/state

then sending a character over UART when the Linux is in sleep to wake it up... This scenario works well.

I want to do the same with CAN, so I enable its wakeup capability:

    $ echo enabled > /sys/class/net/can0/device/power/wakeup

Then put Linux into sleep. It shows that Linux goes into sleep, but it immediately wakes up. I want Linux to be woken up upon the reception of a frame over CAN, just like the UART scenario

Hardware: apalis imx6D ixora v1.2

OS: Linux 5.4.91-33088-g8c05b31a44c3

Question: What could be the problem? How can I do that?

Thanks in advance

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
3,541件の閲覧回数
akbar123
Contributor III

I used NXP Linux kernel from https://source.codeaurora.org/external/imx/linux-imx and the problem fixed

$ git clone https://source.codeaurora.org/external/imx/linux-imx/

$ git checkout -b 4.19 remotes/origin/imx_4.19.35_1.1.0

$ make imx_v7_defconfig
$ make -j$(nproc) zImage
$ make imx6q-apalis-ixora-v1.1.dtb
$ make -j$(nproc) modules

Now I can put Linux into sleep and wake it up by sending a CAN frame to it:

Enable CAN wakeup feature:

$ cd /sys/devices/soc0/soc/2000000.aips-bus/2094000.flexcan/power

$ echo enabled > wakeup

Put Linux into sleep:

$ echo mem > /sys/power/state

Now, by using another board to send a CAN frame, I can wake up Linux

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,595件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Asghar

 

one can try below procedure:

Connect two boards CAN port.

On one board A,

Listen to CAN port.
Enable CAN wakeup:

find /sys -name "wakeup" | grep -i can

e.g.

find /sys -name "wakeup"|grep -i can

/sys/devices/platform/soc/30800000.aips-bus/30a10000.can/power/wakeup

Get all CAN wakeup control points and enable wakeup:

e.g.

echo enabled > /sys/devices/platform/soc/30800000.aips-bus/30a10000.can/power/wakeup

<enable remaining CAN ports too>

 

Suspend the board:

echo mem > /sys/power/state

 

On the other board, send data to CAN port.

Then board A will wake up.

 

Best regards
igor

0 件の賞賛
返信
3,575件の閲覧回数
akbar123
Contributor III

I guess there might be some problem with driver

I tested two different Linux kernel versions available in Toradex Linux built with apalis_imx6_defconfig :

5.4: Linux goes to sleep and immediately wake up

4.9: Linux goes to sleep and does not wake up upon receiving a CAN frame

What kernel version do you use?

0 件の賞賛
返信
3,559件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

may be suggested to try with NXP Sabre SD reference boards.

 

>What kernel version do you use?

 

nxp supports only official linux releases from source.codeaurora.org/external/imx/linux-imx repository
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.70_2.3.0

Documentation

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 件の賞賛
返信
3,542件の閲覧回数
akbar123
Contributor III

I used NXP Linux kernel from https://source.codeaurora.org/external/imx/linux-imx and the problem fixed

$ git clone https://source.codeaurora.org/external/imx/linux-imx/

$ git checkout -b 4.19 remotes/origin/imx_4.19.35_1.1.0

$ make imx_v7_defconfig
$ make -j$(nproc) zImage
$ make imx6q-apalis-ixora-v1.1.dtb
$ make -j$(nproc) modules

Now I can put Linux into sleep and wake it up by sending a CAN frame to it:

Enable CAN wakeup feature:

$ cd /sys/devices/soc0/soc/2000000.aips-bus/2094000.flexcan/power

$ echo enabled > wakeup

Put Linux into sleep:

$ echo mem > /sys/power/state

Now, by using another board to send a CAN frame, I can wake up Linux

0 件の賞賛
返信
3,591件の閲覧回数
akbar123
Contributor III

It has the same result. Linux will go into sleep, BUT it immediately wakes up.

I expect that upon the reception of a CAN frame, It wakes up... But I see something else in practice

0 件の賞賛
返信
3,580件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

this may depend on used hardware, apalis boards are developed and supported

by third party toradex and issue may be posted on community

https://www.toradex.com/community

 

Best regards
igor

 

0 件の賞賛
返信