imx6 3.10.17_1.0.0_ga build device tree

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 3.10.17_1.0.0_ga build device tree

ソリューションへジャンプ
3,326件の閲覧回数
yannickc
Contributor I

Dear all,

I have to do modifications in device tree for the sabresd board I have. As I'm new in dts I do many mistakes before get a correct one.

The problem is that I have to build again all the kernel with bitbake to have my new dtb file and it takes more than 15 minutes each time.

How can I simply build my dts file to generate only the dtb ?

Best regards,

Yannick

ラベル(3)
0 件の賞賛
返信
1 解決策
2,249件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Yannick

     I ran it in the linux-2.6-imx/ directory, it is the first dir when you clone a git repository.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,249件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Yannick

     What is your build command? As far as I know, to only build a dtb file, you can just build it without building kernel, they can be build separately, see below my build command for i.mx6q sabresd board's dtb, hope it helps.

make ARCH=arm CROSS_COMPILE=arm-poky-linux-gnueabi- imx6q-sabresd.dtb;

0 件の賞賛
返信
2,249件の閲覧回数
yannickc
Contributor I

Hi,

Thank you for your quick answer.

I run "bitbake core-image-base". I've already tried to use make command but i've got an error when it is executed. From which directory I should run your command ?

Yannick

0 件の賞賛
返信
2,250件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Yannick

     I ran it in the linux-2.6-imx/ directory, it is the first dir when you clone a git repository.

0 件の賞賛
返信
2,249件の閲覧回数
yannickc
Contributor I

Hi,

I'm sorry for this very late answer. I was busy on other subject. Thank you very much it works for me.

Yannick

0 件の賞賛
返信