Hello,
I've seen a lot of posts in this forum on how to run MCIMX-LVDS touchscreen using ltib. I think I've managed to do this. With minimal distro build I get output of:
lucid@lucid-desktop:~$ sudo cat /dev/input/event2
there are a lot of binary data everytime I touch the screen.
So I took this kernel and applyed it to the ubuntu image that came with the board (dd it to sdcard) and copy compiled kernel modules.
Unfortunately under Ubuntu command:
lucid@lucid-desktop:~$ sudo cat /dev/input/event2
is totally quiet.
The behaviour of touchscreen changed after applying new kernel. Previously after touching it mouse cursor moved to the center of screen. Now it moves to the right bottom corner and generates mouse click (trash folder opens up).
I got:
lucid@lucid-desktop:~$ sudo lsinput
[...]
/dev/input/event2
bustype : BUS_I2C
vendor : 0xeef
product : 0x20
version : 1
name : "eGalax Touch Screen"
phys : "I2C"
bits ev : EV_SYN EV_KEY EV_ABS
[...]
Using evtest I get the event from eGalax but they are always in the same point: (9088, 12224)
lucid@lucid-desktop:~$ sudo evtest /dev/input/event2
Input driver version is 1.0.0
Input device ID: bus 0x18 vendor 0xeef product 0x20 version 0x1
Input device name: "eGalax Touch Screen"
Supported events:
Event type 0 (Sync)
Event type 1 (Key)
Event code 330 (Touch)
Event type 3 (Absolute)
Event code 0 (X)
Value 9088
Min 0
Max 32767
Event code 1 (Y)
Value 12224
Min 0
Max 32767
Event code 24 (Pressure)
Value 0
Min 0
Max 0
Testing ... (interrupt to exit)
eGalax is compiled as part of kernel not module.
Linux image generated by ltib is unusable for early development. Example ubuntu image has everything needed (besides working touchscreen) and working fine.
If someone have already configured MCIMX-LVDS1 to work with example Ubuntu 10.04 please help.
Regards
Maciej Łaski
已解决! 转到解答。
Hello,
so i was easy... you just have to change records in /usr/lib/X11/xorg.conf.d
I deleted files (I do not need them):
/usr/lib/X11/xorg.conf.d/10-evtouch.conf
/usr/lib/X11/xorg.conf.d/10-synaptics.conf
/usr/lib/X11/xorg.conf.d/10-wacom.conf
And changed record in
/usr/lib/X11/xorg.conf.d/05-evdev.conf
to:
lucid@lucid-desktop:~$ cat /usr/lib/X11/xorg.conf.d/05-evdev.conf
# Catchall classes for input devices
# We don't simply match on any device since that also adds accelerometers
# and other devices that we don't really want to use. The list below
# matches everything but joysticks.
Section "InputClass"
Identifier "eGalax"
MatchProduct "eGalax"
MatchDevicePath "/dev/input/event2"
Driver "evdev"
Option "SwapAxes" "off"
Option "Calibration" "0 32767 0 32767"
EndSection
Section "InputClass"
Identifier "evdev pointer catchall"
MatchIsPointer "on"
MatchDevicePath "/dev/input/event7"
Driver "evdev"
EndSection
Section "InputClass"
Identifier "evdev keyboard catchall"
MatchIsKeyboard "on"
MatchDevicePath "/dev/input/event4"
Driver "evdev"
EndSection
I have mouse on event7, keyboard on event4 and touchscreen on event2. Others I don't need.
Hope it will help somebody, and save some time.
Regards
Maciek Łaski
Hello,
so i was easy... you just have to change records in /usr/lib/X11/xorg.conf.d
I deleted files (I do not need them):
/usr/lib/X11/xorg.conf.d/10-evtouch.conf
/usr/lib/X11/xorg.conf.d/10-synaptics.conf
/usr/lib/X11/xorg.conf.d/10-wacom.conf
And changed record in
/usr/lib/X11/xorg.conf.d/05-evdev.conf
to:
lucid@lucid-desktop:~$ cat /usr/lib/X11/xorg.conf.d/05-evdev.conf
# Catchall classes for input devices
# We don't simply match on any device since that also adds accelerometers
# and other devices that we don't really want to use. The list below
# matches everything but joysticks.
Section "InputClass"
Identifier "eGalax"
MatchProduct "eGalax"
MatchDevicePath "/dev/input/event2"
Driver "evdev"
Option "SwapAxes" "off"
Option "Calibration" "0 32767 0 32767"
EndSection
Section "InputClass"
Identifier "evdev pointer catchall"
MatchIsPointer "on"
MatchDevicePath "/dev/input/event7"
Driver "evdev"
EndSection
Section "InputClass"
Identifier "evdev keyboard catchall"
MatchIsKeyboard "on"
MatchDevicePath "/dev/input/event4"
Driver "evdev"
EndSection
I have mouse on event7, keyboard on event4 and touchscreen on event2. Others I don't need.
Hope it will help somebody, and save some time.
Regards
Maciek Łaski
Hi Maciek,
I also try to get the MCIMX-LVDS to work with an imx6 board (SABRE Auto)
at the moment there is no /usr/lib/X11/xorg.conf.d in my build. I built my kernel and rootfs "fsl-image-gui" with YOCTO
Do you know why?
some background informations about the build:
I also get already input data over evtest
Kernel is 3.0.35-4.1.0
X.Org X Server is version 1.14.0