imx53qsb boot up problems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx53qsb boot up problems

3,144 次查看
GiulioBenetti
Contributor I

Hi all,

i've tried with different imx53-QSB (4 in total, all equal) to power on and off very fast.

After 2-3 times imx53 enters Serial Download Mode.

It seems it doesn't recognize right the first 2K on Sd card.

To exit this status there are 2 ways, assert reset or shutdown, also waiting for power supply to die.

I use a hw patch posted here time ago to automatically power up da9053,

anyway even if you use power up button the result is the same.

On errata the only thing I've found was to set bootstrap pins to avoid fast boot and fast sdhc.

This was because of propagation delay on data lines of sd.

To reproduce the problem try to power it up very fast for at least 10 times.

da9053 works fine.

Maybe voltages timing are the problem.

Hope someone can help me.

标记 (1)
0 项奖励
回复
9 回复数

2,844 次查看
roybunce
Contributor II

Thanks Jerry, this solved a problem I posted yesterday - http://imxcommunity.org/group/imx53hardwaredesign/forum/topics/star...

0 项奖励
回复

2,844 次查看
JerryFan
NXP Employee
NXP Employee

Hi,

Please make sure the command "REG_LD_AND_STR_OP(29, 0x0f8, 0x00000800)" included in the flash_header.S

0 项奖励
回复

2,844 次查看
GiulioBenetti
Contributor I

It's flash_header.S shipped with 11.09.

I'm sure it causes the problem.

My board starts up 1 time yes 1 time no.

0 项奖励
回复

2,844 次查看
JerryFan
NXP Employee
NXP Employee

Could you post the flash_header.S file, so we can tell this file caused this issue or not?

I think plug-in should be ok. 

0 项奖励
回复

2,844 次查看
GiulioBenetti
Contributor I

On 11.09 u-boot there is problem on plug-in for booting.

That makes unstable boot process.

I recommend to use old flash_header.S where app pointer is _start:

app_code_jump_v:  .word _start

0 项奖励
回复

2,844 次查看
KrishnaPavan
Contributor II

Hi,

Not only that, but, LTIB uses different cross-compilation tool chains for different versions.

0 项奖励
回复

2,844 次查看
GiulioBenetti
Contributor I

Found.

It was u-boot too new.

With qsb you have to use u-boot from 11.01, using 11.09 makes some problem on reset.

I thought it was bootstrapping, instead it was u-boot doing something wrong, what I don't know.

0 项奖励
回复

2,844 次查看
GiulioBenetti
Contributor I

Do you mean on cfg pins?

I think it's set ok.

The problem is that 4 times on 5 it boot up ok.

But the last it go to serial download mode.

If you have any idea please tell me.

0 项奖励
回复

2,844 次查看
KrishnaPavan
Contributor II

Hi ,

When boot mode is not set properly, it goes to default mode, the serial download mode. Check that..!

0 项奖励
回复