Both MCIMX53-START and MCIMX53-START-R board (aka imx53qsb, LOCO) boards run the Adeneo Android BSP 4.2. Is it possible to put those boards into the STOP mode as the Freescale Application note AN4270 mentions?? We are able to put the boards into the suspend mem mode and the total current consumption drops from 220 mA to 110mA (5V) which is still too much...
Warl0rd
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
The question is still unanswered, but this thread seems abandoned, you are free to close it right now.
AdeneoEmbedded do you have information or can you help with this question?
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.