imx53qsb: STOP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx53qsb: STOP mode

1,270 Views
warl0rd
Contributor I

Both  MCIMX53-START and MCIMX53-START-R board (aka imx53qsb, LOCO) boards run the Adeneo Android BSP 4.2. Is it possible to put those boards into the STOP mode as the Freescale Application note AN4270 mentions?? We are able to put the boards into the suspend mem mode and the total current consumption drops from 220 mA to 110mA (5V) which is still too much...

Tags (3)
0 Kudos
Reply
4 Replies

1,197 Views
YixingKong
Senior Contributor IV

Warl0rd

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

1,197 Views
warl0rd
Contributor I

The question is still unanswered, but this thread seems abandoned, you are free to close it right now.

0 Kudos
Reply

1,197 Views
SergioSolis
NXP Employee
NXP Employee

AdeneoEmbedded do you have information or can you help with this question?

0 Kudos
Reply

1,197 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 Kudos
Reply