yes. but make sure that when acting in 8bit mode, P15~P8 would be used.
please refer to the sentences in RM:
"Each value can be 8-16 bit wide according to configuration of DATA_WIDTH. If DATA_WIDTH is configured to N, then 20-N LSB bits are ignored"
back to the on-the-fly processing, it's another way to process the image.
on-the-fly processing means TVADC->CSI->IC/VDI->...
direct path to memory means TVADC->CSI->SMFC->MEMORY->...