this is my sdp file:
v=0
o=- 0 0 IN IP4 127.0.0.1
s=No Title
c=IN IP4 224.124.0.1/5
t=0 0
a=tool:libavformat 56.30.100
m=video 8000 RTP/AVP 96
b=AS:798
a=rtpmap:96 H264/90000
a=fmtp:96 packetization-mode=1; sprop-parameter-sets=Z2QAIKzZQEAN/qEAAAMAAQAAAwAyjxgxlg==,aOvssiw=; profile-level-id=640020
m=audio 8002 RTP/AVP 97
b=AS:64
a=rtpmap:97 MPEG4-GENERIC/44100/2
a=fmtp:97 profile-level-id=1;mode=AAC-hbr;sizelength=13;indexlength=3;indexdeltalength=3; config=121056E500
i used "gst-launch-0.10 playbin2 uri=file://`pwd`/test1.sdp
WARNING: from element /GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:vbin/GstAutoVideoSink:videosink/MFW_GST_V4LSINK_INFO_T:videosink-actual-sink-mfw_v4l: A lot of buffers are being dropped.
Additional debug info:
/mnt/yocto/bin/fsl-release-bsp/build/tmp/work/armv7a-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r3/gstreamer-0.10.36/libs/gst/base/gstbasesink.c(2875): gst_base_sink_is_too_late (): /GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:vbin/GstAutoVideoSink:videosink/MFW_GST_V4LSINK_INFO_T:videosink-actual-sink-mfw_v4l:
There may be a timestamping problem, or this computer is too slow.
the video output is discontinuous。
could anyone help me,thanks.
Solved! Go to Solution.
Actually only 30 fps is accelerated by the hardware.
So it is the only possible framerate.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I find different framerate frame,as 15、20、24、
but the imx53 received stream framerate is always 30.
I copy the mp4 file to sd card, imx53 could get correct framerate.
0:00:00.971237375 1999 0x10e400 DEBUG mfw_vpudecoder mfw_gst_vpu_decoder.c:4506:mfw_gst_vpudec_setcaps: >>VPU_DEC: set framerate nu 30 de 1
Actually only 30 fps is accelerated by the hardware.
So it is the only possible framerate.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------