imx53_qsb, Android, audio codec, IIM fuses

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx53_qsb, Android, audio codec, IIM fuses

1,285件の閲覧回数
warl0rd
Contributor I

The imx53_qsb (Quickstart-Ripley-B) runs Android 2.3.4 from Adeneo. I've noticed that OMXPlayer somehow uses IIM fuses kernel device "/dev/mxc_iim"

It calls open, mmap, close system calls. After these calls I see a kernel warning:

Unhandled fault: external abort on non-linefetch (0x1018) at 0x2abb2054

If I remove the IIM fuses support from kernel, all the warings "Unhandled fault" are gone

but the sound going out of Freescale SGTL5000 codec becomes really distorted.

I feel that IIM is used in some prebuilt dynamic libraries like lib_omx_player_arm11_elinux.so

But for what purpose?? Why sound becomes broken with the IIM support removed??

ラベル(2)
0 件の賞賛
返信
1 返信

1,157件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Deactivated user, could you please check?

0 件の賞賛
返信