imx53 i2c1 on (PAD_EIM_D21 and PAD_EIM_D28)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx53 i2c1 on (PAD_EIM_D21 and PAD_EIM_D28)

跳至解决方案
1,614 次查看
cyrilcrocquesel
Contributor II

Hi,

I would like on a mx53 QSB the i2c1 on pin :

IMX53_PAD_EIM_D21_I2C1_SCL,

IMX53_PAD_EIM_D28_I2C1_SDA,

I've added this two line in mx53_loco_pads[] in arch/arm/mach-mx5/board-mx53_loco.h (in linux 2.6.38 from freescale). And remove this line :

MX53_PAD_EIM_D21__IPU_DISPB0_SER_CLK,

When the linux boot /dev/i2c-0 is created but I've no signal on scl or sda pin.

What is missing in my modification?

Cordially,

Cyril crocquesel

标签 (1)
0 项奖励
回复
1 解答
986 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For your reference, attached is the BSP porting guide. There is talk about porting I2C. Although it is for i.MX6, the porting is similar to i.MX53.

在原帖中查看解决方案

0 项奖励
回复
1 回复
987 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For your reference, attached is the BSP porting guide. There is talk about porting I2C. Although it is for i.MX6, the porting is similar to i.MX53.

0 项奖励
回复