imx51 wince6 start slow from sdmmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx51 wince6 start slow from sdmmc

Jump to solution
1,275 Views
lee_ee
Contributor II

Dear all
I working on imx51 wince6,OS is boot from eMMC(8G inand),but the system start up consume long time

I follow the debug log to find that OS run OAL layer RTC reset,stop here for long time.

what reason lead to OS start so slow ?

Thanks ahead

0 Kudos
Reply
1 Solution
1,118 Views
justin_jiang
NXP Employee
NXP Employee

Hi Lee_ee,

Since we didn't add log after RTC reset, so you will see it stop on it. Actually it may cost some time on one driver loader. Please add more log on each driver initial function to check which driver cost so long time for boot.

View solution in original post

0 Kudos
Reply
2 Replies
1,119 Views
justin_jiang
NXP Employee
NXP Employee

Hi Lee_ee,

Since we didn't add log after RTC reset, so you will see it stop on it. Actually it may cost some time on one driver loader. Please add more log on each driver initial function to check which driver cost so long time for boot.

0 Kudos
Reply
1,118 Views
lee_ee
Contributor II

thanks

0 Kudos
Reply