hello,everybody,below is my Configuration information
mfgtool.log:
Monday, September 22, 2014 11:54:59
1 - Panel A Start processing SD/MMC <LIST/>.
Panel A Start <CMD/> type="find" body="BootStrap" file="" timeout="60" onError="" text="".
1 - Panel A Finished <CMD/> type="find" body="BootStrap" file="" timeout="60" onError="" text="" SUCCESS code=0x0.
Panel A Start <CMD/> type="init" body="Memory" file="MX51_DDR.xml" timeout="10" onError="" text="".
1 - Panel A Finished <CMD/> type="init" body="Memory" file="MX51_DDR.xml" timeout="10" onError="" text="" SUCCESS code=0x0.
Panel A Start <CMD/> type="load" body="" file="uce.nb0" timeout="10" onError="" text="Doing preLoad."".
1 - Panel A Finished <CMD/> type="load" body="" file="uce.nb0" timeout="10" onError="" text="Doing preLoad."" SUCCESS code=0x0.
Panel A Start <CMD/> type="load" body="" file="eboot_uut.nb0" timeout="10" onError="" text="Loading OS image.".
1 - Panel A Finished <CMD/> type="load" body="" file="eboot_uut.nb0" timeout="10" onError="" text="Loading OS image." SUCCESS code=0x0.
Panel A Start <CMD/> type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. ".
1 - Panel A Finished <CMD/> type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. " SUCCESS code=0x0.
Panel A Start <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="".
Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE
Panel A UtpUpdate Event: VolumeArrival Msg: (null) DevState: Updater OpState: WAITING_FOR_DEVICE
1 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="" SUCCESS code=0x0.
Panel A Start <CMD/> type="push" body="MediaType:SDMMC" file="" timeout="10" onError="" text="Send media type.".
1 - Panel A Finished <CMD/> type="push" body="MediaType:SDMMC" file="" timeout="10" onError="" text="Send media type." SUCCESS code=0x0.
Panel A Start <CMD/> type="push" body="QueryStoreStatus:DSK1:,Timeout:10" file="" timeout="10" onError="" text="Query store status.".
1 - Panel A Finished <CMD/> type="push" body="QueryStoreStatus:DSK1:,Timeout:10" file="" timeout="10" onError="" text="Query store status." FAIL code=0xbad20001.
Panel A: Reason is unknown,failed to run command: type="push" body="QueryStoreStatus:DSK1:,Timeout:10" file="" timeout="10" onError="" text="Query store status."
2 - Panel A Finished processing SD/MMC <LIST/> : FAIL code=-1160642559.
play.ini:
[PROFILE]
PLAYER=MX51 WinCE Update
VERSION=2
[OPERATIONS]
MX_UPDATE=51 RKL MMC WinCE Update,120,0
UTP_UPDATE=OS Firmware,120,1
[OS Firmware]
UCL_INSTALL_SECTION=SD/MMC
[51 RKL MMC WinCE Update]
UCL_INSTALL_SECTION=SD/MMC
serial port Configuration information
com2:115200 8 N 1
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
BSP Clock Configuration:
CKIH = 22579200 Hz
PLL1 = 800000000 Hz
PLL2 = 665000000 Hz
PLL3 = 216000000 Hz
LP_APM = 24000000 Hz
ARM = 800000000 Hz
AXI_A = 166250000 Hz
AXI_B = 133000000 Hz
EMI_SLOW = 133000000 Hz
AHB = 133000000 Hz
IPG = 66500000 Hz
PERCLK = 8000000 Hz
CKIL_SYNC = 32768 Hz
DDR = 200000000 Hz
ARM_AXI = 166250000 Hz
IPU_HSP = 133000000 Hz
VPU_AXI = 166250000 Hz
GPU = 166250000 Hz
GPU2D = 166250000 Hz
DEBUG_APB = 166250000 Hz
ENFC = 26600000 Hz
USBOH3 = 66500000 Hz
ESDHC1 = 47500000 Hz
ESDHC2 = 47500000 Hz
ESDHC3 = 47500000 Hz
ESDHC4 = 47500000 Hz
UART = 24000000 Hz
SSI1 = 5644800 Hz
SSI2 = 5644800 Hz
SSI3 = 5644800 Hz
SSI_EXT1 = 10285714 Hz
SSI_EXT2 = 10285714 Hz
USB_PHY = 24000000 Hz
TVE_216_54 = 216000000 Hz
DI = 27000000 Hz
VPU_RCLK = 24000000 Hz
SPDIF0 = 1142857 Hz
SPDIF1 = 1142857 Hz
SLIMBUS = 66500000 Hz
SIM = 66500000 Hz
FIRI = 24000000 Hz
HSI2C = 66500000 Hz
SSI_LP_APM = 22579200 Hz
SPDIF_XTAL = 24000000 Hz
HSC1 = 216000000 Hz
HSC2 = 216000000 Hz
ESC = 15428571 Hz
CSI_MCLK1 = 24629629 Hz
CSI_MCLK2 = 24629629 Hz
ECSPI = 66500000 Hz
LPSR = 0 Hz
PGC = 66500000 Hz
OSC = 24000000 Hz
CKIH_CAMP1 = 22579200 Hz
CKIH2_CAMP2 = 0 Hz
CKIH2 = 0 Hz
FPM = 33554432 Hz
Microsoft Windows CE Bootloader Common Library Version 1.4 Built Sep 22 2014 10:17:14
INFO: BoardID = 0x0.
Microsoft Windows CE Ethernet Bootloader 1.0 for MX51 EVK (Sep 22 2014 10:23:01)
INFO: SBMR = 0xE060C003.
g_pBSPArgs->g_SDHCBootPort=1;//boot from eSDHC1!
INFO: Bootloader launched from SD.
System ready!
Preparing for download...
BL_JUMP
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
BSP Clock Configuration:
CKIH = 22579200 Hz
PLL1 = 800000000 Hz
PLL2 = 665000000 Hz
PLL3 = 216000000 Hz
LP_APM = 24000000 Hz
ARM = 800000000 Hz
AXI_A = 166250000 Hz
AXI_B = 133000000 Hz
EMI_SLOW = 133000000 Hz
AHB = 133000000 Hz
IPG = 66500000 Hz
PERCLK = 8000000 Hz
CKIL_SYNC = 32768 Hz
DDR = 200000000 Hz
ARM_AXI = 166250000 Hz
IPU_HSP = 133000000 Hz
VPU_AXI = 166250000 Hz
GPU = 166250000 Hz
GPU2D = 166250000 Hz
DEBUG_APB = 166250000 Hz
ENFC = 26600000 Hz
USBOH3 = 66500000 Hz
ESDHC1 = 47500000 Hz
ESDHC2 = 47500000 Hz
ESDHC3 = 47500000 Hz
ESDHC4 = 47500000 Hz
UART = 24000000 Hz
SSI1 = 5644800 Hz
SSI2 = 5644800 Hz
SSI3 = 5644800 Hz
SSI_EXT1 = 10285714 Hz
SSI_EXT2 = 10285714 Hz
USB_PHY = 24000000 Hz
TVE_216_54 = 216000000 Hz
DI = 27000000 Hz
VPU_RCLK = 24000000 Hz
SPDIF0 = 1142857 Hz
SPDIF1 = 1142857 Hz
SLIMBUS = 66500000 Hz
SIM = 66500000 Hz
FIRI = 24000000 Hz
HSI2C = 66500000 Hz
SSI_LP_APM = 22579200 Hz
SPDIF_XTAL = 24000000 Hz
HSC1 = 216000000 Hz
HSC2 = 216000000 Hz
ESC = 15428571 Hz
CSI_MCLK1 = 24629629 Hz
CSI_MCLK2 = 24629629 Hz
ECSPI = 66500000 Hz
LPSR = 0 Hz
PGC = 66500000 Hz
OSC = 24000000 Hz
CKIH_CAMP1 = 22579200 Hz
CKIH2_CAMP2 = 0 Hz
CKIH2 = 0 Hz
FPM = 33554432 Hz
Windows CE Kernel for ARM (Thumb Enabled) Built on May 7 2012 at 12:47:43
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
OEMInit: silicon r呝?偮蓚j???V)?偮羠jOALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
WARNING: SRTC was reset.
BSPPmicInit start .
BSPPmicInit end .
+OALIoCtlQueryBoardId ()g_dwBoardID = 0
+OALIoCtlQueryBoardId ()g_dwBoardID = 0
BOT_InternalInit with Drivers\Active\13
Exception 'Data Abort' (4): Thread-Id=01ef0002(pth=9272a63c), Proc-Id=00400002(pprc=80749308) 'NK.EXE', VM-active=01aa0002(pprc=965f596c) 'udevice.exe'
PC=c01d409c(gwes.dll+0x0005409c) RA=c01d4084(gwes.dll+0x00054084) SP=d07cfdd8, BVA=00000104
UFN_ATTACH with key = Drivers\Active\13
UFN_CONFIGURED: BOT_OpenInterface again
UTP command:Media type: SDMMC.
UTP command:QueryStoreStatus.
UTP command:Check if disk is ready.
Please be patient to wait...
Send storage disk name: DSK1:.
Send time out: 10.
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
ERROR:UceCommandDeal fail.
where is my error for looking at my printed information?In this process, the SD card to mount the drive letter appears on the screen of the computer, but also cannot format or cannot be opened?What can i do?Help me,Please!!
解決済! 解決策の投稿を見る。
Hi Arctic
KLM8G2FE3B is eMMC 4.41 verson while i.MX51 eSDHC supports up to rev.4.2 only
as decribed in sect.31.1.1 "Features" MCIMX51RM MCIMX51 Multimedia Applications Processor
SD/MMC driver checks for chip revision and may not work properly if it is not designed for
support of particular revision. So suggest to check with another chips.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Before wrong operation,I can boot wince6.0 from SD/MMC normally,but OS didn‘t display SD folder "SD memory".So I want to deal with it,Below is my wrong operation
Booting IMX51 from SD/MMC(klm8g2fe3b-b001)
After seting wrong eboot menu information ,cause the system can't start any more,I look for lots of forum or blog,they all can't solve my question.how shoud can i do?
If you could write with ATK you can continue to use it.
~igor