imx477 sensor driver for i.MX8M-Plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx477 sensor driver for i.MX8M-Plus

跳至解决方案
10,709 次查看
malik_cisse
Senior Contributor I

Hi,

I am writing imx477 sensor driver for i.mx8m-plus based on some preexisting driver in kernel_source_code/drivers/media/i2c/imx319.c (which is part of official linux kernel)

Unfortunatelly I get some kernel error: "mxc-md: probe of 32c00000.bus:camera failed with error -515"

As can be seen in dmesg shippet below.

I have the feeling that some system callback functions aremissing.

Any insight? Thank you

 

dmesg output:

...

[ 3.229148] bus: 'i2c': driver_probe_device: matched device 2-001a with driver imx477
[ 3.229153] bus: 'i2c': really_probe: probing driver imx477 with device 2-001a
[ 3.229181] imx477 2-001a: no pinctrl handle
[ 3.229209] imx477 2-001a: ########## Probing IMX477 Driver ##########
[ 3.236113] link-frequencies 0 value 450000000
[ 3.240597] imx477 2-001a: 2-001a supply VANA not found, using dummy regulator
[ 3.247872] devices_kset: Moving 2-001a to end of list
[ 3.247876] PM: Moving i2c:2-001a to end of list
[ 3.247883] imx477 2-001a: Linked as a consumer to regulator.0
[ 3.247897] imx477 2-001a: 2-001a supply VDIG not found, using dummy regulator
[ 3.255179] imx477 2-001a: 2-001a supply VDDL not found, using dummy regulator
[ 3.273479] imx477 2-001a: $$$ Read I2C: IMX477 CHIP ID = 477 $$$
[ 3.279644] imx477 2-001a: ########## End Probing IMX477##########
[ 3.285839] driver: 'imx477': driver_bound: bound to device '2-001a'
[ 3.285844] devices_kset: Moving 2-001a to end of list
[ 3.285851] PM: Moving i2c:2-001a to end of list
[ 3.285877] bus: 'i2c': really_probe: bound device 2-001a to driver imx477

...

[ 3.660712] platform 32c00000.bus:camera: Retrying from deferred list
[ 3.661350] bus: 'platform': driver_probe_device: matched device 32c00000.bus:camera with driver mxc-md
[ 3.661358] bus: 'platform': really_probe: probing driver mxc-md with device 32c00000.bus:camera
[ 3.661376] mxc-md 32c00000.bus:camera: no pinctrl handle
[ 3.661518] device: 'video0': device_add
[ 3.661570] PM: Adding info for No Bus:video0
[ 3.661672] mx8-img-md: Registered mxc_isi.0.capture as /dev/video0
[ 3.668100] mx8-img-md: Registered sensor subdevice: imx477 2-001a (1)
[ 3.674700] mx8-img-md: created link [mxc_isi.0] => [mxc_isi.0.capture]
[ 3.681355] mx8-img-md: created link [mxc-mipi-csi2.0] => [mxc_isi.0]
[ 3.687817] mx8-img-md: subdev_notifier_complete error exit
[ 3.693453] mxc-md 32c00000.bus:camera: Sensor register failed
[ 3.699324] mxc-md: probe of 32c00000.bus:camera failed with error -515

0 项奖励
回复
1 解答
10,660 次查看
malik_cisse
Senior Contributor I

Hi,

I finally solved the missing callback function issue.

One needs to implement dummy ".link_setup" callback function returning 0. The system is expecting this callback. This is a bug in the Kernel driver.

static const struct media_entity_operations ar0144_entity_ops = {
.link_setup = ar0144_link_setup,
};

 

static int ar0144_link_setup(struct media_entity *entity,
struct media_pad const *local,
struct media_pad const *remote,
u32 flags)
{

return 0;
}

在原帖中查看解决方案

10 回复数
9,239 次查看
Goko_gr
Contributor I

Hi Malik,

Thanks a lot for your answer. We are also using iMX8MP and i wonder which driver file name have you modified and made the link operation ? In our case, we found a similar code part as yours, but it already returns zero.

static const struct media_entity_operations csi_entity_ops = {
.link_setup = csi_link_setup,
.link_validate = v4l2_subdev_link_validate,
.get_fwnode_pad = csi_get_fwnode_pad,
};

 

static int csi_link_setup(struct media_entity *entity,
const struct media_pad *local,
const struct media_pad *remote, u32 flags)
{

struct v4l2_subdev *sd = media_entity_to_v4l2_subdev(entity);
struct csi_priv *priv = v4l2_get_subdevdata(sd);
struct v4l2_subdev *remote_sd;
int ret = 0;

dev_dbg(priv->dev, "link setup %s -> %s\n", remote->entity->name,
local->entity->name);

mutex_lock(&priv->lock);

if (local->flags & MEDIA_PAD_FL_SINK) {
if (!is_media_entity_v4l2_subdev(remote->entity)) {
ret = -EINVAL;
goto out;
}

remote_sd = media_entity_to_v4l2_subdev(remote->entity);

if (flags & MEDIA_LNK_FL_ENABLED) {
if (priv->src_sd) {
ret = -EBUSY;
goto out;
}
priv->src_sd = remote_sd;
} else {
priv->src_sd = NULL;
}

goto out;
}

/* this is a source pad */

if (flags & MEDIA_LNK_FL_ENABLED) {
if (priv->sink) {
ret = -EBUSY;
goto out;
}
} else {
v4l2_ctrl_handler_free(&priv->ctrl_hdlr);
v4l2_ctrl_handler_init(&priv->ctrl_hdlr, 0);
priv->sink = NULL;
/* do not apply IC burst alignment in csi_try_crop */
priv->active_output_pad = CSI_SRC_PAD_IDMAC;
goto out;
}

/* record which output pad is now active */
priv->active_output_pad = local->index;

/* set CSI destination */
if (local->index == CSI_SRC_PAD_IDMAC) {
if (!is_media_entity_v4l2_video_device(remote->entity)) {
ret = -EINVAL;
goto out;
}

if (priv->fim) {
ret = imx_media_fim_add_controls(priv->fim);
if (ret)
goto out;
}

priv->dest = IPU_CSI_DEST_IDMAC;
} else {
if (!is_media_entity_v4l2_subdev(remote->entity)) {
ret = -EINVAL;
goto out;
}

remote_sd = media_entity_to_v4l2_subdev(remote->entity);
switch (remote_sd->grp_id) {
case IMX_MEDIA_GRP_ID_IPU_VDIC:
priv->dest = IPU_CSI_DEST_VDIC;
break;
case IMX_MEDIA_GRP_ID_IPU_IC_PRP:
priv->dest = IPU_CSI_DEST_IC;
break;
default:
ret = -EINVAL;
goto out;
}
}

priv->sink = remote->entity;
out:
//return 0;    //The part that we have added.
mutex_unlock(&priv->lock);
return ret;
}

 

 

In this structure, we have modified the csi_link_setup just as you did, but there is no change. So, it would be very helpful if you share your driver file, ofc if you still have it or do you have any recommendation to solve this issue by changing exactly which part of the driver file.

Thanks again, have a nice day.

 

 

0 项奖励
回复
9,229 次查看
malik_cisse
Senior Contributor I

Hi,
Unfortunately I cannot share the code because I am under NDA.

I do understand your frustration though since the debug logs often doe not indicate actual root cause.

0 项奖励
回复
9,257 次查看
Goko_gr
Contributor I

Hi Malik,

We've got the same subdev_notifier_complete error exit with adv7280 chip. No NXP employees have supported us so far as expected, so if you can help us about our issue as well, it would be very appreciated. Thanks for your help. You can find the link of our issue below.

https://community.nxp.com/t5/i-MX-Processors/iMX8MP-MIPI-CSI2-Problem-with-ADV7280-and-Camera/m-p/14...

0 项奖励
回复
9,250 次查看
malik_cisse
Senior Contributor I

Hi,

This is long time ago.

Not sure how I solved this particular issue.

One of the key factors was that I needed to implement callback functions that are needed in the imx8mp BSP which are not present in other drivers.

For example .link_setup callback was missing but no error indicated that as you can see further in this thread.
One idea is to take a known functioning driver (e.g Basler) and check if all callbacks there are implemented in your own driver.

0 项奖励
回复
10,653 次查看
malik_cisse
Senior Contributor I

Thank you Igor. 

Yes, Basler Cam is definitelly a good source of knowledge to get started.

Do you know if one can buy the NXP devkit + Basler cam?

Thx, Malik

0 项奖励
回复
10,661 次查看
malik_cisse
Senior Contributor I

Hi,

I finally solved the missing callback function issue.

One needs to implement dummy ".link_setup" callback function returning 0. The system is expecting this callback. This is a bug in the Kernel driver.

static const struct media_entity_operations ar0144_entity_ops = {
.link_setup = ar0144_link_setup,
};

 

static int ar0144_link_setup(struct media_entity *entity,
struct media_pad const *local,
struct media_pad const *remote,
u32 flags)
{

return 0;
}

10,671 次查看
gghy
Contributor I

Hi, i'm having the same problem with a imx334 sensor, if i find anything useful i will keep you updated

0 项奖励
回复
10,692 次查看
malik_cisse
Senior Contributor I

I will look at those examples.

Thank you Igor

Malik

0 项奖励
回复