imx287的USB设备读写速度问题

cancel
Showing results for 
Search instead for 
Did you mean: 

imx287的USB设备读写速度问题

676 Views
bratzhang
Contributor II
Dear Sir:
      客户现在在用imx287的USB设备读写这块遇到了速度瓶颈。
具体情况如下:
      我们修改了内核代码中的f_hid.c对应的读操作的代码,然后用上位机测试程序连续发20M数据,通过bus hound监测,速度大约为900KB/S.     f_hid.c封装了read接口给linux应用层调用,linux应用程序使用select监控文件句柄进行读操作。通过测试比较每个数据包的包号,发现在发送2M数据之后(我做了大约1M的KFIFO的队列缓存),开始出现大量丢包。
    
     如果我修改上位机测试程序,每发送一个数据包,增加2 ms的延时,则数据不会出现丢失。但USB写的速度从原来的900KB/S 降到127KB/S。这样的速度无法进行音视频传输,基于此情况, 我修改了f_hid.c我能想到很多情况,经过验证还是会丢包。希望您能给我一些提示,或者方法。万分感谢。附件为修改后的f_hid.c。
        用的高速的口,PC端使用的是libusb的无驱设计,输入报文长度为64字节,输出报文长度为1024个字节。使用HID的方式进行数据收发。
使用的是高速USB的描述符。不知道有什么建议没有?
Labels (2)
0 Kudos
4 Replies

336 Views
bratzhang
Contributor II

any good suggestion? ? hope for your response asap. 

0 Kudos

336 Views
jimmychan
NXP TechSupport
NXP TechSupport

I didn’t test the HID like that. I am thinking you may reach the data rate limitation of the HID class.

0 Kudos

336 Views
jimmychan
NXP TechSupport
NXP TechSupport

which BSP are you using?

0 Kudos

336 Views
bratzhang
Contributor II

cat /proc/version 
Linux version 2.6.35.3-571-gcca29a0 (root@ubuntu) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #92 PREEMPT Wed Oct 25 02:47:46 CST 2017

0 Kudos