imx28 yocto build gstreamer video playback not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx28 yocto build gstreamer video playback not working

跳至解决方案
1,766 次查看
michaeldonahoe
Contributor II

I've built an image using Yocto set on the daisy branch and I'm unable to play videos using gstreamer.  Audio works fine though.

Linux imx28evk 2.6.35.3-maintain+yocto+g903363e #1 PREEMPT Tue Jun 17 07:52:05 PDT 2014 armv5tejl GNU/Linux

gst-launch -v playbin2 uri=file:///test.mp4

Setting pipeline to PAUSED ...

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: ring-buffer-max-size = 0

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: buffer-size = -1

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: buffer-duration = -1

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: use-buffering = FALSE

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: download = FALSE

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: uri = "file:///test.mp4"

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: connection-speed = 0

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0: source = (GstFileSrc) source

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstTypeFindElement:typefind.GstPad:src: caps = video/quicktime, variant=(string)iso

Pipeline is PREROLLING ...

Aiur: 3.0.11

Core: MPEG4PARSER_06.07.04  build on Dec  5 2013 19:49:20

  mime: video/quicktime; audio/x-m4a; application/x-3gp

  file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm9_elinux.so.3.2

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAiurDemux:aiurdemux0.GstPad:sink: caps = video/quicktime, variant=(string)iso

Content Info:

  URI:

       file:///test.mp4

  Idx File:

       /home/root/.aiur/.test.mp4.aidx

  Seekable  : Yes

  Size(byte): 83869253

Movie Info:

  Seekable  : Yes

  Live      : No

  Duration  : 0:02:19.711664000

  ReadMode  : Track

  Track     : 2

Track 00 [video_000000] Enabled

  Duration: 0:02:19.596672000

  Language: und

  Mime:

       video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=

       (fraction)24000/1001

Track 01 [audio_000000] Enabled

  Duration: 0:02:19.711664000

  Language: und

  Mime:

       audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)1

       27536, framed=(boolean)true, stream-format=(string)raw, codec_data=(buffer)11905

       6e500

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0: max-size-buffers = 5

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0: max-size-time = 0

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0: max-size-bytes = 2097152

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0.GstPad:sink0: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0.GstPad:src0: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstH264Parse:h264parse0.GstPad:src: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001, stream-format=(string)byte-stream, alignment=(string)au

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstH264Parse:h264parse0.GstPad:src: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001, stream-format=(string)byte-stream, alignment=(string)au

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstH264Parse:h264parse0.GstPad:sink: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAacParse:aacparse0.GstPad:src: caps = audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)127536, framed=(boolean)true, stream-format=(string)raw, codec_data=(buffer)119056e500

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAacParse:aacparse0.GstPad:sink: caps = audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)127536, framed=(boolean)true, stream-format=(string)raw, codec_data=(buffer)119056e500

H264D_ARM9_02.06.03  build on Apr 16 2013 13:34:03.

MFW_GST_H264_DECODER_PLUGIN 3.0.11 build on Jun 23 2014 09:19:33.

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001, stream-format=(string)byte-stream, alignment=(string)au

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001, stream-format=(string)byte-stream, alignment=(string)au

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0: max-size-buffers = 5

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0: max-size-time = 0

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0: max-size-bytes = 2097152

/GstPlayBin2:playbin20/GstInputSelector:inputselector0.GstSelectorPad:sink0: always-ok = FALSE

/GstPlayBin2:playbin20/GstInputSelector:inputselector1.GstSelectorPad:sink0: always-ok = FALSE

/GstPlayBin2:playbin20/GstInputSelector:inputselector1: active-pad = (GstSelectorPad) sink0

/GstPlayBin2:playbin20/GstInputSelector:inputselector0: active-pad = (GstSelectorPad) sink0

MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Jun 23 2014 09:19:24.

/GstPlayBin2:playbin20/GstPlaySink:playsink0: volume = 1.000000

/GstPlayBin2:playbin20/GstPlaySink:playsink0: mute = FALSE

/GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:abin/GstAutoAudioSink:audiosink/GstAlsaSink:audiosink-actual-sink-alsa: ts-offset = 0

/GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:vbin/GstAutoVideoSink:videosink/MFW_GST_V4LSINK_INFO_T:videosink-actual-sink-mfw_v4l: ts-offset = 0

/GstPlayBin2:playbin20/GstInputSelector:inputselector0.GstSelectorPad:sink0: tags = ((GstTagList*) 0x41461220)

/GstPlayBin2:playbin20/GstInputSelector:inputselector0.GstSelectorPad:sink0: tags = ((GstTagList*) 0x41461250)

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/MFW_GST_H264DEC_INFO_T:mfw_gst_h264dec_info_t0.GstPad:sink: caps = video/x-h264, parsed=(boolean)true, width=(int)1280, height=(int)720, framerate=(fraction)24000/1001, stream-format=(string)byte-stream, alignment=(string)au

/GstPlayBin2:playbin20/GstInputSelector:inputselector1.GstSelectorPad:sink0: tags = ((GstTagList*) 0x30598)

Beep: 3.0.11

Core: AAC decoder Wrapper  build on Jan 22 2014 15:42:57

  mime: audio/mpeg, mpegversion=(int){2,4}

  file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm9_elinux.so.3

CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.07.00_ARM9  build on Sep 18 2013 10:31:41.

ERROR: from element /GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/MFW_GST_H264DEC_INFO_T:mfw_gst_h264dec_info_t0: fatal error

Additional debug info:

non recoverable error while decoding the H.264 Data

ERROR: pipeline doesn't want to preroll.

Setting pipeline to NULL ...

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstBeepdec1:beepdec10.GstPad:sink: caps = audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)127536, framed=(boolean)true, stream-format=(string)raw, codec_data=(buffer)119056e500

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0.GstGhostPad:src1: caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)16, depth=(int)16, rate=(int)48000, channels=(int)2

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20.GstDecodePad:src1: caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)16, depth=(int)16, rate=(int)48000, channels=(int)2

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstBeepdec1:beepdec10.GstPad:src: caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)16, depth=(int)16, rate=(int)48000, channels=(int)2

/GstPlayBin2:playbin20/GstInputSelector:inputselector1.GstSelectorPad:sink0: tags = ((GstTagList*) 0x105ab0)

/GstPlayBin2:playbin20/GstInputSelector:inputselector1.GstSelectorPad:sink0: caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)16, depth=(int)16, rate=(int)48000, channels=(int)2

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0.GstGhostPad:src1.GstProxyPad:proxypad11: caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)16, depth=(int)16, rate=(int)48000, channels=(int)2

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20.GstDecodePad:src1.GstProxyPad:proxypad8: caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)16, depth=(int)16, rate=(int)48000, channels=(int)2

/GstPlayBin2:playbin20/GstInputSelector:inputselector1.GstPad:src: caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)16, depth=(int)16, rate=(int)48000, channels=(int)2

Total rendered:0

/GstPlayBin2:playbin20/GstInputSelector:inputselector1.GstSelectorPad:sink0: caps = NULL

/GstPlayBin2:playbin20/GstInputSelector:inputselector1.GstPad:src: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0.GstGhostPad:src1: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20.GstDecodePad:src1: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/MFW_GST_H264DEC_INFO_T:mfw_gst_h264dec_info_t0.GstPad:sink: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstCapsFilter:capsfilter0.GstPad:src: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstCapsFilter:capsfilter0.GstPad:sink: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstH264Parse:h264parse0.GstPad:src: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstH264Parse:h264parse0.GstPad:sink: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstBeepdec1:beepdec10.GstPad:src: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstBeepdec1:beepdec10.GstPad:sink: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAacParse:aacparse0.GstPad:src: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAacParse:aacparse0.GstPad:sink: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0.GstPad:sink1: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0.GstPad:src1: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0.GstPad:sink0: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstMultiQueue:multiqueue0.GstPad:src0: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAiurDemux:aiurdemux0.GstPad:audio_000000: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAiurDemux:aiurdemux0.GstPad:video_000000: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAiurDemux:aiurdemux0.GstPad:sink: caps = NULL

/GstPlayBin2:playbin20/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstTypeFindElement:typefind.GstPad:src: caps = NULL

[--->FINALIZE v4l_sink

[--->FINALIZE aiurdemux

Freeing pipeline ...

标签 (1)
0 项奖励
回复
1 解答
1,500 次查看
michaeldonahoe
Contributor II

Resolved this issue turns out something was up with the sample files I was using.  They all played in the virtual machine fine but had issues on the 28.  I have Qt 5 and g-streamer working now.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,501 次查看
michaeldonahoe
Contributor II

Resolved this issue turns out something was up with the sample files I was using.  They all played in the virtual machine fine but had issues on the 28.  I have Qt 5 and g-streamer working now.

0 项奖励
回复