imx28, what's the best bsp?

cancel
Showing results for 
Search instead for 
Did you mean: 

imx28, what's the best bsp?

931 Views
katte
Contributor II

What's the best BSP for imx28 available now?

I've tried the 2.6.35_1.1.0_130130 BSP, but it have a lot of missing or broken packages.

Maybe is possible to use yocto?

Labels (3)
0 Kudos
3 Replies

526 Views
katte
Contributor II

Thanks to all for the info.

Can I follow this guide https://community.freescale.com/docs/DOC-94849

to have "yocto" working on my custom board?

0 Kudos

526 Views
gary_bisson
Senior Contributor III

Hi Marco,

Yes you can use Yocto to get the best out of the i.MX28. Here is the machine config file:

meta-fsl-arm/imx28evk.conf at master · Freescale/meta-fsl-arm · GitHub

Note that it is using linux-fslc which is the community kernel based on the Linux kernel 4.1.

meta-fsl-arm/mxs-base.inc at master · Freescale/meta-fsl-arm · GitHub

meta-fsl-arm/linux-fslc_4.1.bb at master · Freescale/meta-fsl-arm · GitHub

Regards,

Gary

0 Kudos

526 Views
igorpadykov
NXP TechSupport
NXP TechSupport

HI Marco

one can look at i.MX28 community BSPs

Public images - fsl-community-bsp/master/526/x11

https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/arch/arm/boot/dts/imx28-evk.dts...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos