imx28 mmcblk0: retrying using single block read

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 mmcblk0: retrying using single block read

2,380 Views
shashikanthirem
Contributor III

Hi all,

i am using kernel 2.6.35.10, 

i am calling statvfs("/mnt/mmcblk0p1", &info); with a gap of 500ms in a while(1); -- > this is to get the status of various size like used , free, and available space

but when i do sd card remove and plug it back i am seeing a huge error on terminal

[ 83.160000] mmcblk0: retrying using single block read
[ 83.160000] mmcblk0: error -110 sending status comand
[ 83.180000] mmcblk0: error -110 sending read/write command, response 0xb00, c
[ 83.180000] end_request: I/O error, dev mmcblk0, sector 6688
[ 83.220000] mmcblk0: error -110 sending status comand
[ 83.220000] mmcblk0: error -110 sending read/write command, response 0xb00, c
[ 83.240000] end_request: I/O error, dev mmcblk0, sector 6689
[ 83.250000] mmcblk0: error -110 sending status comand
[ 83.250000] mmcblk0: error -110 sending read/write command, response 0xb00, c
[ 83.270000] end_request: I/O error, dev mmcblk0, sector 6690
[ 83.280000] mmcblk0: error -110 sending s

it keeps on populating, nearly 30 sec an udev rule gets an eject event, on removal of sd card ,

any one face this pls share your thought

patch would be helpful, i need a patch in kernel version, now i cannot move to new kernel

Labels (1)
0 Kudos
Reply
2 Replies

2,296 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shashikant

kernel 2.6.35.10 is outdated kernel and not more supported by nxp,

support with it can be provided with Commercial Support and Engineering Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,296 Views
shashikanthirem
Contributor III

hi all

any update ?

0 Kudos
Reply