imx28 fresh board usb boot from linux host

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx28 fresh board usb boot from linux host

1,667 次查看
bibinb
Contributor I

i have a fresh custom board with imx28 with USB as the only first time boot option. Is there any tool to boot imx28 from linux host PC(preferably ubuntu).

标签 (2)
0 项奖励
回复
3 回复数

1,383 次查看
fabio_estevam
NXP Employee
NXP Employee

You can use mxsldr:

3.1.5 USB Firmware Upload | www.denx-cs.de/doku

Regards,

Fabio Estevam

0 项奖励
回复

1,383 次查看
igorpadykov
NXP Employee
NXP Employee

Hi bibin

one can try mfg tool for programming fresh board with usb

Programmers (Flash, etc.) (8)

Tool and documentation for downloading i.MX28 image during manufacturing (REV L2.6.35_1.1.0)

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,383 次查看
bibinb
Contributor I

Thanks igor for the reply.

This tool will work only in Windows OS. Right?

Is there any tool available for ubuntu or other linux distros?

0 项奖励
回复