imx28 DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx28 DMA

跳至解决方案
2,518 次查看
liuxing
Contributor II

Does the DMA of imx28 support memory- to-memory transfer?I mean that transfer data block in DDR.

pastedImage_1.png

标签 (1)
0 项奖励
回复
1 解答
2,442 次查看
igorpadykov
NXP Employee
NXP Employee

> address of channel 0~13 is constant.Is it right?

yes, right.

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,442 次查看
liuxing
Contributor II

If the dest and source address can be programmed,the memory to memory access can be implemented.

what's about PIOWORD?

The CMDPIOWORDS field, if nonzero,
instructs the DMA engine to copy these words to the APB, beginning at the first
register address offset for the peripheral and and incrementing the register offset each
cycle.

0 项奖励
回复
2,443 次查看
igorpadykov
NXP Employee
NXP Employee

> address of channel 0~13 is constant.Is it right?

yes, right.

Best regards
igor

0 项奖励
回复
2,442 次查看
igorpadykov
NXP Employee
NXP Employee

Hi xing

I believe you are right, dma does not support memory to memory transfers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,442 次查看
liuxing
Contributor II

I think the dest/source address of channel 0~13 is constant.Is it right?

If I want to access the whole physical memory,do you have a way to implement it?I wanted to implement it via DMA.

0 项奖励
回复
2,442 次查看
liuxing
Contributor II

Thanks a lot!

Are you sure this conclusion?what's the function of the empty channel?

0 项奖励
回复