Hi Guys,
I finally manage to get my new board running imx27 using Linux 3.9.4 with all devices ready to run.
I2C and ov2460 + mx_camera load and detect properly.
Now I want to test the VPU and the new features for V4Lv2 and find out that I must have the firmware
firmware for the VPU (former: vpu_fw_imx27_TO2.bin) but with the new kernel its comes with a new version
called v4l-codadx6-imx27.bin.
Did freescale support developers and make this firmware available?
Thanks
and kind regards
Chris
Hello Fabio,
is there an official Freescale repository where we can get these i.MX27/5/6 VPU firmwares for vanilla kernels ? (with automated wget scripts for example)
What is the license of these binaries ? Are we allowed to redistribute them ?
Regards,
Julien
Hi Julien,
Currently only the firmwares for FSL kernels are available from FSL BSPs.
Regards,
Fabio Estevam
Fabio,
I'll tried the firmware load today ;-) using Linux 3.9.6
INIT: version 2.88 booting
[info] Using makefile-style concurrent boot in runlevel S.
[....] Starting the hotplug events dispatcher: udevd[ 6.779818] udevd[722]: starting version 175
. ok
[....] Synthesizing the initial hotplug events...[ 7.979742] coda coda-imx27.0: Initialized CodaDx6.
[ 7.984672] coda coda-imx27.0: Firmware version: 2.2.5
[ 8.082520] coda coda-imx27.0: codec registered as /dev/video0
[ 8.753523] usbcore: registered new interface driver btusb
done.
successfully loaded!
Thanks
Message was edited by: Chris Ruehl
Hi, now I'm a step further after fix the I2C bus and have my OV2640 running.
To capture I used a modified version of
gcc -O2 -g -Wall mxc_v4l2_capture.c -o bin.x
and its seams that the v4l not yet stable ..
root@gtsir-nand:~# ./bin.x -w 640 -h 480 -c 100 /var/www/a.yuv
g_width = 640, g_height = 480
[ 8770.853104] mx2-camera imx27-camera.0: Camera driver attached to camera 0
--------------------------------------------------------------------------------------------
Width = 640 Height = 480 Image size = 460800
pixelformat = 842093913 colorspace = 7
--------------------------------------------------------------------------------------------
buf.index 0
buf.index 1
[ 8786.382831] mx2-camera imx27-camera.0: Camera driver detached from camera 0
but this is something I have to communicate with the guys take care of the codaDX6.
Cheers Chris
Fabio,
Thank you very much, I wait a long time to get it. I will let you know how that works for me.
It is possible to get the firmware for the imx53 too, I have an other project in the queue working with this SOC for Video on Demand?
Regards,
Chris Ruehl
Hi Chris,
Unfortunately I only saw your post today.
About mx53, I think you will find this patch series very useful:
http://www.mail-archive.com/linux-media@vger.kernel.org/msg63391.html
It was posted today and allows 1080p playback on mx53.
I will check which is the appropriate firmware that can be used on mx53 as well.
Regards,
Fabio Estevam
Hi Fabio,
The current coda driver in linux kernel 3.16 requests a firmware named "v4l-coda7541-imx53.bin" for IMX53.
I couldn't find it anywhere. I tried to rename the firmware in IMX53 BSP from /lib/firmware/vpu/vpu_fw_imx53.bin to v4l-coda7541-imx53.bin, but i guess it is wrong format. The following message is displayed by dmesg
coda 63ff4000.vpu: firmware get command error
coda 63ff4000.vpu: HW initialization failed
Can you provide a link for the correct IMX53 coda firmware ?
Best Regards,
Ronaldo Moura
Fabio,
Thanks again for your quick reply ;-)
Yes indeed, this patch serious looking very interesting to me too. Good hint!
Regards
Chris
Hi Chris,
we made the patches Fabio pointed to in this thread; there is more ongoing work which is not ready for mainline yet but of course already available for project work. So if we can help, please drop me a note at sales@pengutronix.de.
Regards,
Robert
Hi Robert,
sure I'm happy to help testing the patches. My problem , I run a production this Jun/July. If shipment is done I have my head free for this.
Chris
Freescale Team! No answers for me?
Chris
Hi Chris,
I read this with interest since I'm at a similar point. I looked at the byte/half order between the coda driver and the original FSL VPU driver and wrote a little program to dump the bit_code2 array to file. Looking at vpu_fw_imx7_TO2.bin it seems it has a version/size header and the 16-bit words are swapped. I think the file should begin with these bytes in hex...
22 00 0e e4 90 e1 ...
Having said this, I still haven't got the FW to load correctly, but I think this is a problem with my udev setup and userspace FW loader.
May I ask, how are you going to drive the coda device? Have you found a GStreamer plugin for it?
IanJ.
Hi Ian,
tried the file you mentioned already renamed to v4l-codadx6-imx27.bin, and the firmware got loaded but spit out an other error message. I opened a service request and have a 1st response, the sales team wants to contact me on this.
For the Gstreamer its works on the V4L interface. Once the video/firmware is loaded you are able to talk to the VPU by IOCTRL commands for example to rotate the image ...
I let you know when I have a progress here.
Chris