imx25 internal RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx25 internal RAM

跳至解决方案
1,770 次查看
rbruce
Contributor II

I would like to load and execute a program in the imx25 internal RAM, either via the serial downloader or from SPI flash.  Is this possible?

I am assuming some portions of internal RAM are used by the ROM code and would be off limits.  I don't find much information on internal RAM in the imx25 reference manual.

标签 (1)
0 项奖励
回复
1 解答
1,624 次查看
Yuri
NXP Employee
NXP Employee

Hope the enclosed example helps.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,625 次查看
Yuri
NXP Employee
NXP Employee

Hope the enclosed example helps.

0 项奖励
回复
1,624 次查看
rbruce
Contributor II

OK. I’m running a small program from internal RAM based on the sample you sent .

Thanks very much for your help.

Robert W. (Bill) Bruce

Watlow

Winona, MN

0 项奖励
回复
1,624 次查看
rbruce
Contributor II

Yuri,

Thanks for the example. After a quick look at the files, I think this will help me accomplish what I want to do.

Robert W.(Bill) Bruce

Watlow

Winona, MN

0 项奖励
回复