imx-yocto-L4.14.98_2.0.0_ga中xwayland环境中,无法使用qtvirtualkeyboard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx-yocto-L4.14.98_2.0.0_ga中xwayland环境中,无法使用qtvirtualkeyboard

ソリューションへジャンプ
3,269件の閲覧回数
liangyan
Contributor III

我在imx6qsabresd平台中,编译的xwayland桌面环境中无法使用qtvirtualkeyboard,无法弹出qtvirtualkeyboard。我换了一个warrior,qtvirtualkeyboard键盘能弹出来,但是会出现闪退?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,250件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

 

We are working on MX6Sabre board and there is no lagging on the system and L5.4.24. There is yocto sumo but we are talking about the QT.

 

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,257件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello liangyang,

 Qtvirtualkeyboard is working on MX6 and L5.4.24 BSP, However if you like to support in chromium the QtWebEngine as you could run it in EGLFS and avoid all the boilerplate of X environment. This could also rely on a QML virtual keyboard. You need go to the yocto community:

http://freescale.github.io/

 

Regards

 

0 件の賞賛
返信
3,255件の閲覧回数
liangyan
Contributor III

hello Bio_TICFSL

我验证过了,如果使用EGLFS话,在framework环境中,我运行Qt webengine的simplebrowser是比较卡顿的,webview界面卡顿,所以,我采用的的是xwayland环境,能保证Qt webengine运行是不卡顿的,但是又没法弹出虚拟键盘。

你说的 L5.4.24 BSP,这个在framework的EGLFS环境是可以弹出虚拟键盘,而且simplebrowser是运行不卡顿的吗?

我当时选择sumo是因为它是一个GA版本,L5.4.24也是一个GA版本啊吗?

0 件の賞賛
返信
3,251件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

 

We are working on MX6Sabre board and there is no lagging on the system and L5.4.24. There is yocto sumo but we are talking about the QT.

 

Regards

 

0 件の賞賛
返信