imx usb loader issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx usb loader issue

2,934 Views
JeevanTRaj
Contributor I

Hi

We have developed a surveillance camera product based on imx6s processor. For the purpose of device production flashing, we are using the processor USB and imx_usb loader software utility. In some of our device the usb_loader is showing some error related to the dl_command and hence the device is not getting flashed. While the rest of the majority of the devices are getting flashed in this setup without this particular error. We ensured that the board is working fine. The failed board's USB is identified on the PC(Freescale Semiconductor, Inc. i.MX  6Solo 6DualLite SystemOnChip in RecoveryMode) and listed properly when given the command lsusb on the host PC.

Attached are the prints from the USB loader.

We have to fix the problem of these boards immediately. Any help to resolve this issue will be appreciated.

@igorpadykov 

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

2,907 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

 

imx_usb loader is community utility, not supported by nxp. NXP supports only uuu tool

https://github.com/NXPmicro/mfgtools

In general one can recheck imx_usb loader usage as described below

https://variwiki.com/index.php?title=Imx_usb_loader

and post issue on   https://github.com/boundarydevices/imx_usb_loader/issues

 

Best regards
igor

2,933 Views
JeevanTRaj
Contributor I
 
0 Kudos
Reply